Problems about Vector Table Remapping of KV11 Series:

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problems about Vector Table Remapping of KV11 Series:

1,503 Views
Saiwenliang
Contributor II
Recently, I have a project to implement IAP function on kv11, but I can't find the operation instructions for remapping the interrupt vector table. After checking the reference manual, I found that there is a register VTOR used to control the offset of  the interrupt vector table, but i couldn't find the operation about VTOR from the driver library. How can I remap the interrupt vector table? 
 
It's better to show me the detailed sequence, thanks.
0 Kudos
Reply
1 Reply

1,496 Views
nxf56274
NXP Employee
NXP Employee

Hi,

You can refer this link.  https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDMK64F-SD-Bootloader/ta-p/1099807. Notice the figure 9.

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply