Problem using KWIKSTIK-K40

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Problem using KWIKSTIK-K40

跳至解决方案
1,898 次查看
hardeepsingh
Contributor II

I'm using Kinetis KWIKSTIK-K40 demo board where I'm facing problems while programming the device. When I connect it say USB device not recognized. Tried to give the path of the .inf file for driver but it did not install the driver and hence, I'm not able to program the Flash on the device. Please suggest what shall I do to resolve it.

标签 (2)
0 项奖励
回复
1 解答
1,688 次查看
CarlosCasillas
NXP Employee
NXP Employee

Hello,

Have you ensured which Kwikstik version do you have? Have you verified if this case corresponds to the described on “KWIKSTIK_07: Failure to Power from J-Link USB” section of the KwikStik-K40 Hardware Errata Rev. 5 document, available at the following link:

www.freescale.com/files/32bit/doc/errata/KWIKSTIKK40HWER.pdf


Hope this will be useful for you.

Best regards!

/Carlos

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,689 次查看
CarlosCasillas
NXP Employee
NXP Employee

Hello,

Have you ensured which Kwikstik version do you have? Have you verified if this case corresponds to the described on “KWIKSTIK_07: Failure to Power from J-Link USB” section of the KwikStik-K40 Hardware Errata Rev. 5 document, available at the following link:

www.freescale.com/files/32bit/doc/errata/KWIKSTIKK40HWER.pdf


Hope this will be useful for you.

Best regards!

/Carlos

0 项奖励
回复