Problem using KWIKSTIK-K40

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem using KWIKSTIK-K40

ソリューションへジャンプ
1,899件の閲覧回数
hardeepsingh
Contributor II

I'm using Kinetis KWIKSTIK-K40 demo board where I'm facing problems while programming the device. When I connect it say USB device not recognized. Tried to give the path of the .inf file for driver but it did not install the driver and hence, I'm not able to program the Flash on the device. Please suggest what shall I do to resolve it.

ラベル(2)
0 件の賞賛
返信
1 解決策
1,689件の閲覧回数
CarlosCasillas
NXP Employee
NXP Employee

Hello,

Have you ensured which Kwikstik version do you have? Have you verified if this case corresponds to the described on “KWIKSTIK_07: Failure to Power from J-Link USB” section of the KwikStik-K40 Hardware Errata Rev. 5 document, available at the following link:

www.freescale.com/files/32bit/doc/errata/KWIKSTIKK40HWER.pdf


Hope this will be useful for you.

Best regards!

/Carlos

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,690件の閲覧回数
CarlosCasillas
NXP Employee
NXP Employee

Hello,

Have you ensured which Kwikstik version do you have? Have you verified if this case corresponds to the described on “KWIKSTIK_07: Failure to Power from J-Link USB” section of the KwikStik-K40 Hardware Errata Rev. 5 document, available at the following link:

www.freescale.com/files/32bit/doc/errata/KWIKSTIKK40HWER.pdf


Hope this will be useful for you.

Best regards!

/Carlos

0 件の賞賛
返信