Parallel NOR flash connection with MK64, Data write error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Parallel NOR flash connection with MK64, Data write error

2,573件の閲覧回数
NEIL4
Contributor II

SchematicSchematicWaveform: CS,ALE,OE,WE,ADDRESS_0Waveform: CS,ALE,OE,WE,ADDRESS_0

I have interfaced 16bit NOR flash(SST39LF802C) with MK64 via Latch (54ABT16373A), the connections are made as per the above diagram. Programming had done as per App. Note(AN4393).

During read, write and erase, the OE and CS are always at HIGH logic state. Due to which could not able to perform any operation on the flash. Any feedback is really helpful. Thank you!

0 件の賞賛
返信
3 返答(返信)

2,534件の閲覧回数
vicentegomez
NXP TechSupport
NXP TechSupport

Can you check that there is not any hardware issue?

 

Maybe you have an open pin

 

Regards

 

0 件の賞賛
返信

2,528件の閲覧回数
NEIL4
Contributor II

Can you check that there is not any hardware issue?

Maybe you have an open pin

-->

1. The GPIO toggle works fine at the Flash end, So don't think so any open air. But any Read and Write doesnot work.

0 件の賞賛
返信

2,520件の閲覧回数
vicentegomez
NXP TechSupport
NXP TechSupport

Hi

So you can send data from the K64, the gpio can send the information only the driver for the NOR is not working

 

Please check that the configurations are correct, I do not know if there is any special set for your NOR Flash

 

 

0 件の賞賛
返信