Parallel NOR flash connection with MK64, Data write error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Parallel NOR flash connection with MK64, Data write error

2,573 次查看
NEIL4
Contributor II

SchematicSchematicWaveform: CS,ALE,OE,WE,ADDRESS_0Waveform: CS,ALE,OE,WE,ADDRESS_0

I have interfaced 16bit NOR flash(SST39LF802C) with MK64 via Latch (54ABT16373A), the connections are made as per the above diagram. Programming had done as per App. Note(AN4393).

During read, write and erase, the OE and CS are always at HIGH logic state. Due to which could not able to perform any operation on the flash. Any feedback is really helpful. Thank you!

0 项奖励
回复
3 回复数

2,534 次查看
vicentegomez
NXP TechSupport
NXP TechSupport

Can you check that there is not any hardware issue?

 

Maybe you have an open pin

 

Regards

 

0 项奖励
回复

2,528 次查看
NEIL4
Contributor II

Can you check that there is not any hardware issue?

Maybe you have an open pin

-->

1. The GPIO toggle works fine at the Flash end, So don't think so any open air. But any Read and Write doesnot work.

0 项奖励
回复

2,520 次查看
vicentegomez
NXP TechSupport
NXP TechSupport

Hi

So you can send data from the K64, the gpio can send the information only the driver for the NOR is not working

 

Please check that the configurations are correct, I do not know if there is any special set for your NOR Flash

 

 

0 项奖励
回复