PID algorithm in SDK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,789件の閲覧回数
leonardomoreno
Contributor II

Hello, my name Leonardo Moreno and I'm trying to use de FRDM-KE06Z board to control the temperature of a Peltier Cell through PWM. For doing this, I'm going to use a PID controller.

I'm new to the Kinetis boards, and therefore I'm having a bit of confusión while developing the Project.

In this post: [Kinetis M] High Precision PID controller there is a mention that the PID algorithms are already provided for the kinetis boards in SDK software tolos.

I downloaded the SDK 2.0 of a similar board (FRDM-K64F) in hopes of having a look at the PID algorithms, but I can't seem to find them anywhere.

Can anybody please guide me as to where can I find the algorithms? Do they come as an application example?

Many thanks,

Leonardo Moreno

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
3,017件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Leonardo,

    PID is an algorithm, it is not depend on the chip.

    Our KSDK have give the PID algorithm code for your reference, I already attached it, you don't need to use the whole KSDK project, because the KE06 don't have the KSDK now, it has the according sample code driver for your reference, you can download it from this link:

FRDM-KEXX Driver Library Package

    When you want to use the PID algorithm, you can call the PID function in the attachment.

Wish it helps you!
Have a great day,
Jingjing

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
3,018件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Leonardo,

    PID is an algorithm, it is not depend on the chip.

    Our KSDK have give the PID algorithm code for your reference, I already attached it, you don't need to use the whole KSDK project, because the KE06 don't have the KSDK now, it has the according sample code driver for your reference, you can download it from this link:

FRDM-KEXX Driver Library Package

    When you want to use the PID algorithm, you can call the PID function in the attachment.

Wish it helps you!
Have a great day,
Jingjing

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
3,017件の閲覧回数
leonardomoreno
Contributor II

Excellent, thank you Jing

0 件の賞賛
返信