Open Source JTAG with IAR ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Open Source JTAG with IAR ?

Jump to solution
1,741 Views
joelesco
Contributor III

Hi,

I'm just trying the  IAR Embedded Workbench IDE. When I want to download the code on the TWR-K70 do I need a J-link or like CW there 'is  an Open Source JTAG solution ?

I'm looking forward to your answer !

0 Kudos
Reply
1 Solution
1,625 Views
antonioconcio
NXP Employee
NXP Employee

Hi Jay,

Yeah you can use On-board JTAG debug circuit. You have only to check in your project that PE Micro is selected in Debugger tab and then OSJTag is set as hardware interface in PE micro tab, see screenshot below.

pippo Screenshot - 11_20_2013 , 11_35_15 AM.png

Best Regards,

Antonio

View solution in original post

0 Kudos
Reply
1 Reply
1,626 Views
antonioconcio
NXP Employee
NXP Employee

Hi Jay,

Yeah you can use On-board JTAG debug circuit. You have only to check in your project that PE Micro is selected in Debugger tab and then OSJTag is set as hardware interface in PE micro tab, see screenshot below.

pippo Screenshot - 11_20_2013 , 11_35_15 AM.png

Best Regards,

Antonio

0 Kudos
Reply