On the flash programming

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

On the flash programming

ソリューションへジャンプ
2,805件の閲覧回数
pietrodicastri
Senior Contributor II

Good morning

I have a serious problem of customer assistance. I need to update remotely the software on the target board. He has the JTAG

but I don t find a way to update using only the binary ELF or HEX. From the KDS it is necessary to work with the project and expose the source code.

I cannot to do so. So I need someone's solution to use the JTAG with only the binary.

Thank You

Pietro

タグ(2)
0 件の賞賛
返信
1 解決策
2,719件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Pietro,

you don't need the sources, you can simply flash the file with the 'Flash from file...' function

pastedImage_0.png

Another way is to use the GDB command line (see Command Line Programming and Debugging with GDB | MCU on Eclipse ).

Or simply use a dummy project and in the debug configuration specify the binary you want to download:

pastedImage_2.png

I hope this helps,

Erich

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,720件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Pietro,

you don't need the sources, you can simply flash the file with the 'Flash from file...' function

pastedImage_0.png

Another way is to use the GDB command line (see Command Line Programming and Debugging with GDB | MCU on Eclipse ).

Or simply use a dummy project and in the debug configuration specify the binary you want to download:

pastedImage_2.png

I hope this helps,

Erich

0 件の賞賛
返信
2,718件の閲覧回数
pietrodicastri
Senior Contributor II

After a lot of tries I manage to get through the process.

It seems I need always to go in SWD even my hardware does not need, and use some magic numbers.

I don t thing it is supporting the CYCLONE now..

Thank You

Pietro

0 件の賞賛
返信
2,718件の閲覧回数
pietrodicastri
Senior Contributor II

Hi Erich

I tried your suggestions. but the flash from file does not work.

I just use the Main tab, I specify in the Project a name, and the file name. When I try to flash the progress bar they proceed until the end.

But the board does not start the application.

I tried also to manipulate the settings in the other tab pages. But I get no results.

I need a deeper guideline to use the programmer.

Thank You for the support

Pietro

0 件の賞賛
返信