Need TSI sample code for FRDM-KL25Z

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Need TSI sample code for FRDM-KL25Z

2,818件の閲覧回数
bhavinmaru
Contributor III

Hello, does someone have used TSI of KL25z Board without Processor Expert and could post some code please.

0 件の賞賛
返信
3 返答(返信)

2,421件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Bhavin,

   Except the KSDK tsi code in you another post,  you still can use the old sample code for FRDM-KL25:

http://www.nxp.com/assets/downloads/data/en/lab-test-software/KL25_SC.exe 

After you download and install it, you can find the TSI code in folder:

kl25_sc_rev10\klxx-sc-baremetal\build\iar\FRDM_KL25ZDemo

Wish it helps you!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,421件の閲覧回数
bhavinmaru
Contributor III

Hello,

Is there any update on this?

Any help in this will be appreciated more.

0 件の賞賛
返信

2,421件の閲覧回数
mjbcswitzerland
Specialist V

Hi

You have been given code and links in your other thread asking for the same thing: https://community.nxp.com/thread/439833 
There is also a link to a binary image that shows it all in operation on the board that you are using.

Regards

Mark

0 件の賞賛
返信