Mass erase is disabled for k series

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Mass erase is disabled for k series

1,465 次查看
jyothi_pula
Contributor I

Hi All,

Using segger debug tool performed erase chip. After performing the task microcontroller got into protected mode. it isnot allowing to flash source again the showing " couldn't find the core  in coresight setup. Abort the setup."

If I browse it google it mentioned chip could be blocked. Help me to unlock the chip.

Thanks in advance.

Best regards,

Jyothi Pula.

标签 (1)
0 项奖励
回复
1 回复

1,365 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Jyothi Pula,

Please refer: How To Sucessfully Program a Custom made Kinetis Microcontroller Board.(If this doesn't work, then please try to use the P&E recovery utility mentioned in Bricking and Recovering FRDM-KL25Z Boards: Reset, SWD Clock and Low Power.)

 

Check the hardware circuit of your custom board.(NMI_b \ Reset_b \ debug pins)

Please download the MCUXpresso IDE, step8 can be replaced by resurrect locked Kinetis device in GUI Flash Tool.

 

 

GUI Flash Tool extended for P&E and SEGGER

The GUI Flash Tool previously was only for the LinkServer (or LPC-Link2) connections.

GUI Flash Tool

GUI Flash Tool

Now it supports all debug probe connections, including P&E and SEGGER, and I can program, erase or even resurrect a ‘bricked’ Kinetis device:

linkserver-gui-flash-tool.png

LinkServer GUI Flash Tool

PEMicro GUI Flash Tool

PEMicro GUI Flash Tool

Segger GUI Flash Tool

Segger GUI Flash Tool

Using the toolbar icon is probably the most convenient way to use the GUI Flash Programmer, it is possible to run it from the debugger launch configuration too:

Running GUI Flash Programmer from Launch Configuration

Running GUI Flash Programmer from Launch Configuration

The operation executed is logged in the Console View:

GUI Flash Tool Console Output

GUI Flash Tool Console Output

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复