MY FRDM-K64F doesn't work

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MY FRDM-K64F doesn't work

1,420件の閲覧回数
cyx
Contributor I

it is the first time i use this board. After being connected with computer by USB, the RGB LED keeps flickering and the teraterm can't show any character string even after modify the configration.

And after build a project in KDS, I can't debug. It always shows an error as follow:

An internal error occurred during: "Launching LED_Debug_OpenOCD".

ilg.gnuarmeclipse.debug.gdbjtag.dsf.GnuArmServicesFactory.<init>(Ljava/lang/String;Ljava/lang/String;)V

could someone help me? I'm new to this development board

0 件の賞賛
返信
1 返信

1,310件の閲覧回数
ivadorazinova
NXP Employee
NXP Employee

Hi yx chen,

thank you for your feedback.

Please, see this post​ if you don´t have issue with the GNU ARM Eclipse plugin.

For this case is needed to replace original files. It is known issue, for this moment it is a workaround.

For your first steps I can recommend you:

Kinetis Design Studio Videos, Part 1: Installation of KDS and Kinetis SDK

Kinetis Design Studio Videos, Part 2: Installation of OpenSDA Firmware on Freedom Board

Kinetis Design Studio Videos, Part 3: Debugging with Kinetis Design Studio

Kinetis Design Studio Videos, Part 4: Using Processor Expert in KDS

Please let me know, if this helps you.

Best Regards,

Iva

0 件の賞賛
返信