MKM35Z512VLL7's UART PORT OPEN DRAIN

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MKM35Z512VLL7's UART PORT OPEN DRAIN

ソリューションへジャンプ
1,823件の閲覧回数
jun1
Contributor V

HI.

Use UART1 by connecting the RS485 driver IC to the outside. Is it necessary to disable open drain when using it with the UART function (I don't use it as an open drain)?
Pin Control Register n (PORTx_PCRn). 5 ODE    ---    Open Drain Enable

thank you.

 

ラベル(1)
0 件の賞賛
返信
1 解決策
1,805件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi,

I think it is base on what RS485 interface chip do you use. If you select MAX3485 for example, DI & RD is not open drain. So you can't set it to open drain mode.

 

Regards,

Jing

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,806件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi,

I think it is base on what RS485 interface chip do you use. If you select MAX3485 for example, DI & RD is not open drain. So you can't set it to open drain mode.

 

Regards,

Jing

0 件の賞賛
返信