MKM35Z512VLL7's UART PORT OPEN DRAIN

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MKM35Z512VLL7's UART PORT OPEN DRAIN

Jump to solution
1,798 Views
jun1
Contributor V

HI.

Use UART1 by connecting the RS485 driver IC to the outside. Is it necessary to disable open drain when using it with the UART function (I don't use it as an open drain)?
Pin Control Register n (PORTx_PCRn). 5 ODE    ---    Open Drain Enable

thank you.

 

Labels (1)
0 Kudos
Reply
1 Solution
1,780 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi,

I think it is base on what RS485 interface chip do you use. If you select MAX3485 for example, DI & RD is not open drain. So you can't set it to open drain mode.

 

Regards,

Jing

View solution in original post

0 Kudos
Reply
1 Reply
1,781 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi,

I think it is base on what RS485 interface chip do you use. If you select MAX3485 for example, DI & RD is not open drain. So you can't set it to open drain mode.

 

Regards,

Jing

0 Kudos
Reply