MKL25Z128 Internal USB 3.3V regulator limitations

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MKL25Z128 Internal USB 3.3V regulator limitations

Jump to solution
1,243 Views
MAPC
Senior Contributor I

Hello,

Can I use the MKL25Z1128 USB 3.3V regulator to power the MCU, if I don't surpass Iout = 120mA?

Thanks,

Marco Coelho

Labels (1)
0 Kudos
Reply
1 Solution
1,143 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi Marco,

Yes, you can use KL25 USB regulator 3.3V output to power the KL25 chip, please refer the application below:

2015-09-24_10-41-35.png

Wish it helps.


Have a great day,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,144 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi Marco,

Yes, you can use KL25 USB regulator 3.3V output to power the KL25 chip, please refer the application below:

2015-09-24_10-41-35.png

Wish it helps.


Have a great day,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply