MKL04Z8VLC4 programming

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MKL04Z8VLC4 programming

跳至解决方案
5,829 次查看
joevignola
Contributor III

When using CodeWarrior 10.4 and 10.3 I can erase and partially program the chip on my bare board.  I used the same elf file and programmer to load simple program onto the kl05 freedom board without any problems.

Any help would be greatly appreciated.

Joe

标签 (1)
标记 (1)
1 解答
5,080 次查看
joevignola
Contributor III

Turns out that there was a bug in the P&E micro algorithm for the KL04Z8 chip.  Here is the one that they sent me but I'm sure they will post an update on their web site.

there was an error in the processor expert code too, which had the wrong starting address for the RAM.

freescale_kl04z8m4_1x32x2k_pflash.arp

;version 1.02, 06/05/2013, Copyright P&E Microcomputer Systems, www.pemicro.com [mk_8k_n_pflash_m0]

;device freescale, kl04z8m4, 1x32x2k, desc=pflash

;begin_cs device=$00000000, length=$00002000, ram=$20000000

;end_cs

REQUIRES_PROG_VERSION=1.03/

NO_ON_CHIP_RAM

DO_MASS_ERASE_AND_RESET ;Perform MDM Mass erase

NO_TIMING_TEST

WRITE_LONG=0000A000/F000300C/ ; turn off speculation and cache

WRITE_LONG=FFFFFFFF/40020010/ ;All PFlash protection off

WRITE_LONG=00000000/40048100/ ; turn off watchdog timer

BLANK_MODULE_ONLY

BOUNDARY_MASK=FFFFFC00/

BLOCKING_MASK=00000003/

NO_BASE_ADDRESS=00000000/

ADDR_RANGE=00000000/00001FFF/00/FFFFFFFC/FFFFFC00/ ; $00000000-$00001FFF P-Flash

TEST_VALUE=00/0000040C/00000033/00000020/00/003/007/Data that is about to be programmed will permanently secure the device. Continue?/

TEST_VALUE=00/0000040C/00000033/00000021/00/003/007/Data that is about to be programmed will permanently secure the device. Continue?/

TEST_VALUE=00/0000040C/00000033/00000023/00/003/007/Data that is about to be programmed will permanently secure the device. Continue?/

ICS_RANGE=000312500/000390625/000006400/ ICS Range (LSB = decimal place)

09BIT_TRIM=40064002/40064003/01/000003FF/000003FE/01400000/

USER=SD Secure Device 0 /00000000/00000000/

S01800006D6B5F386B5F6E5F70666C6173685F6D302E7331395C

S315200000000C0100200C01002000010000000000006F

S315200000100020000000000000640000200000000016

S3152000002000000000620000208A0000208A000020D4

S315200000304E00002050000020540000200000000048

S315200000400000000000000000CA00002000BE00BE24

S3152000005000BE0000214D70262E702A787026324070

S3152000006000BE00BE224E234F234C00211F4A8A4643

S315200000700B88891CB24503D1A34205D1921EF6E70F

S31520000080BB4201D1921EF2D100BE144669600626FB

S31520000090EE711E782E725B1C1E786E725B1C1E78AB

S315200000A0AE725B1C1E78EE725B1C80262E7000BF23

S315200000B02E7880221640FBD02E787022164003D14F

S315200000C0091D241FE2D1002200BE0422064B084F40

S315200000D03C68044E26401E600549D6E700000240D3

S315200000E0FEFFFFFFFCFFFFFF0C01002000200000A9

S311200000F00C040000FFFF0000FEFF0000D3

S70520000000DA

¥F

在原帖中查看解决方案

0 项奖励
回复
9 回复数
5,081 次查看
joevignola
Contributor III

Turns out that there was a bug in the P&E micro algorithm for the KL04Z8 chip.  Here is the one that they sent me but I'm sure they will post an update on their web site.

there was an error in the processor expert code too, which had the wrong starting address for the RAM.

freescale_kl04z8m4_1x32x2k_pflash.arp

;version 1.02, 06/05/2013, Copyright P&E Microcomputer Systems, www.pemicro.com [mk_8k_n_pflash_m0]

;device freescale, kl04z8m4, 1x32x2k, desc=pflash

;begin_cs device=$00000000, length=$00002000, ram=$20000000

;end_cs

REQUIRES_PROG_VERSION=1.03/

NO_ON_CHIP_RAM

DO_MASS_ERASE_AND_RESET ;Perform MDM Mass erase

NO_TIMING_TEST

WRITE_LONG=0000A000/F000300C/ ; turn off speculation and cache

WRITE_LONG=FFFFFFFF/40020010/ ;All PFlash protection off

WRITE_LONG=00000000/40048100/ ; turn off watchdog timer

BLANK_MODULE_ONLY

BOUNDARY_MASK=FFFFFC00/

BLOCKING_MASK=00000003/

NO_BASE_ADDRESS=00000000/

ADDR_RANGE=00000000/00001FFF/00/FFFFFFFC/FFFFFC00/ ; $00000000-$00001FFF P-Flash

TEST_VALUE=00/0000040C/00000033/00000020/00/003/007/Data that is about to be programmed will permanently secure the device. Continue?/

TEST_VALUE=00/0000040C/00000033/00000021/00/003/007/Data that is about to be programmed will permanently secure the device. Continue?/

TEST_VALUE=00/0000040C/00000033/00000023/00/003/007/Data that is about to be programmed will permanently secure the device. Continue?/

ICS_RANGE=000312500/000390625/000006400/ ICS Range (LSB = decimal place)

09BIT_TRIM=40064002/40064003/01/000003FF/000003FE/01400000/

USER=SD Secure Device 0 /00000000/00000000/

S01800006D6B5F386B5F6E5F70666C6173685F6D302E7331395C

S315200000000C0100200C01002000010000000000006F

S315200000100020000000000000640000200000000016

S3152000002000000000620000208A0000208A000020D4

S315200000304E00002050000020540000200000000048

S315200000400000000000000000CA00002000BE00BE24

S3152000005000BE0000214D70262E702A787026324070

S3152000006000BE00BE224E234F234C00211F4A8A4643

S315200000700B88891CB24503D1A34205D1921EF6E70F

S31520000080BB4201D1921EF2D100BE144669600626FB

S31520000090EE711E782E725B1C1E786E725B1C1E78AB

S315200000A0AE725B1C1E78EE725B1C80262E7000BF23

S315200000B02E7880221640FBD02E787022164003D14F

S315200000C0091D241FE2D1002200BE0422064B084F40

S315200000D03C68044E26401E600549D6E700000240D3

S315200000E0FEFFFFFFFCFFFFFF0C01002000200000A9

S311200000F00C040000FFFF0000FEFF0000D3

S70520000000DA

¥F

0 项奖励
回复
5,080 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Joe Vignola,

Do you mean "When using CodeWarrior 10.4 and 10.3 I can not erase and partially program the chip on my bare board. "? would you please help to clarify? Thanks for your patience!!

B.R

Kan

0 项奖励
回复
5,080 次查看
joevignola
Contributor III

I get a successful result from erasing the chip but I get an error returned when programming.  I have added the log messages below.

Thanks, Joe.

GDI: DiMeeDisconnect(exec_env_id = 1)

GDI: => DI_OK

GDI: DiGdiClose()

GDI: => DI_OK

=== CodeWarrior GDI protocol log ===

GDI DLL: C:\Freescale\CW MCU v10.4\MCU\bin\Plugins\Debugger\protocols\..\..\support\arm\gdi\arm_pne_gdi.dll

CPU: KL04Z8M4

GDI: DiGdiOpen()

GDI: => DI_OK

GDI: DiGdiGetFeatures()

GDI: => DI_OK

GDI: Identification: ARM Cortex M4 P&E to GDI wrapper, Version: 1.0.1, MeeAvailable: true, NrCpusAvailable: 1

GDI: DiGdiAddCallBack(cb_type = 0x4000)

GDI: => DI_OK

GDI: DiGdiInitIO()

GDI: Mtwks Callback(MTWKS_CB_SETMEEID, 1) => DI_OK

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : CWDBG, Entry : LaunchConfiguration, Value : KL04_Test_FLASH_PnE U-MultiLink, R) => DI_OK

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : PEDEBUG, Entry : DO_DEBUG_OUTPUT, Value : HFSUIDFH5390FJIfnsdofnfjsdoiFHSIDO, R) => DI_ERR_NONFATAL

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : PEDEBUG, Entry : DEPENDENCY_CHECK, Value : HFSUIDFH5390FJIfnsdofnfjsdoiFHSIDO, R) => DI_ERR_NONFATAL

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : PEDEBUG, Entry : UUID, Value : HFSUIDFH5390FJIfnsdofnfjsdoiFHSIDO, R) => DI_ERR_NONFATAL

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : CWDBG, Entry : Processor, Value : KL04Z8M4, R) => DI_OK

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : PEDEBUG, Entry : ERASE_PROGRAM_WITHOUT_ASKING, Value : 0, R) => DI_OK

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : PEDEBUG, Entry : AUTO_SYNC, Value : 1, R) => DI_OK

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : PEDEBUG, Entry : DOTRIM, Value : 1, R) => DI_OK

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : PEDEBUG, Entry : CURRENT_ALGORITHM_INDEX, Value : 0, R) => DI_OK

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : PEDEBUG, Entry : PRESERVE1_START, Value : 0, R) => DI_OK

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : PEDEBUG, Entry : PRESERVE1_END, Value : 3, R) => DI_OK

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : PEDEBUG, Entry : PRESERVE1_ACTIVE, Value : 0, R) => DI_OK

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : PEDEBUG, Entry : PRESERVE2_START, Value : 0, R) => DI_OK

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : PEDEBUG, Entry : PRESERVE2_END, Value : 3, R) => DI_OK

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : PEDEBUG, Entry : PRESERVE2_ACTIVE, Value : 0, R) => DI_OK

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : PEDEBUG, Entry : PRESERVE3_START, Value : 0, R) => DI_OK

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : PEDEBUG, Entry : PRESERVE3_END, Value : 3, R) => DI_OK

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : PEDEBUG, Entry : PRESERVE3_ACTIVE, Value : 0, R) => DI_OK

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : KL04Z8M4, Entry : PRESERVE_EEPROM_START, Value : HFSUIDFH5390FJIfnsdofnfjsdoiFHSIDO, R) => DI_ERR_NONFATAL

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : KL04Z8M4, Entry : PRESERVE_EEPROM_END, Value : HFSUIDFH5390FJIfnsdofnfjsdoiFHSIDO, R) => DI_ERR_NONFATAL

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : KL04Z8M4, Entry : PRESERVE_EEPROM, Value : HFSUIDFH5390FJIfnsdofnfjsdoiFHSIDO, R) => DI_ERR_NONFATAL

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : PEDEBUG, Entry : ALTERNATIVE_ALGORITHM_PATH, Value : HFSUIDFH5390FJIfnsdofnfjsdoiFHSIDO, R) => DI_ERR_NONFATAL

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : PEDEBUG, Entry : ALTERNATIVE_ALGORITHM_CHECKBOX, Value : 0, R) => DI_OK

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : PEDEBUG, Entry : PARTITION_PARAM, Value : HFSUIDFH5390FJIfnsdofnfjsdoiFHSIDO, R) => DI_ERR_NONFATAL

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : PEDEBUG, Entry : DO_PARTITIONING, Value : HFSUIDFH5390FJIfnsdofnfjsdoiFHSIDO, R) => DI_ERR_NONFATAL

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : PEDEBUG, Entry : CUSTOM_TRIM, Value : 0, R) => DI_OK

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : KL04Z8M4, Entry : TRIM_VALUE, Value : HFSUIDFH5390FJIfnsdofnfjsdoiFHSIDO, R) => DI_ERR_NONFATAL

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : PEDEBUG, Entry : NGS_TRIM_OVERRIDE_REFERENCE_FREQUENCY, Value : 3276800, R) => DI_OK

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : PEDEBUG, Entry : ENABLE_FLASH_PROGRAMMING_DIALOG, Value : 1, R) => DI_OK

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : STARTUP, Entry : SPECIFY_NETWORKCARD_ENABLED, Value : 0, R) => DI_OK

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : STARTUP, Entry : IO_DELAY_CNT, Value : HFSUIDFH5390FJIfnsdofnfjsdoiFHSIDO, R) => DI_ERR_NONFATAL

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : STARTUP12, Entry : show_hstep_assembly_details, Value : HFSUIDFH5390FJIfnsdofnfjsdoiFHSIDO, R) => DI_ERR_NONFATAL

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : CWDBG, Entry : Connect, Value : 0, R) => DI_OK

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : STARTUP, Entry : eclipse_show_connection_assistant, Value : HFSUIDFH5390FJIfnsdofnfjsdoiFHSIDO, R) => DI_ERR_NONFATAL

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : STARTUP, Entry : FREQ_FX, Value : 4, R) => DI_OK

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : STARTUP, Entry : FREQ_NORMAL, Value : 9, R) => DI_OK

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : STARTUP, Entry : FREQ_OSJTAG, Value : 0, R) => DI_OK

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : STARTUP, Entry : FREQ_CYCLONE, Value : 3, R) => DI_OK

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : STARTUP, Entry : FREQ_TRACELINK, Value : 3, R) => DI_OK

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : STARTUP, Entry : FREQ_LIGHTNING, Value : HFSUIDFH5390FJIfnsdofnfjsdoiFHSIDO, R) => DI_ERR_NONFATAL

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : STARTUP, Entry : FREQ_OPENSDA, Value : 0, R) => DI_OK

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : STARTUP, Entry : RESET_DELAY, Value : 0, R) => DI_OK

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : STARTUP, Entry : PORT, Value : 21, R) => DI_OK

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : STARTUP, Entry : interface_selection, Value : 1, R) => DI_OK

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : PORT, Entry : IP, Value : HFSUIDFH5390FJIfnsdofnfjsdoiFHSIDO, R) => DI_ERR_NONFATAL

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : STARTUP, Entry : USE_CYCLONEPRO_RELAYS, Value : 0, R) => DI_OK

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : STARTUP, Entry : CyclonePro_poweroffonexit, Value : 0, R) => DI_OK

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : STARTUP, Entry : CyclonePro_currentvoltage, Value : 128, R) => DI_OK

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : STARTUP, Entry : CyclonePro_PowerDownDelay, Value : 250, R) => DI_OK

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : STARTUP, Entry : CyclonePro_PowerUpDelay, Value : 250, R) => DI_OK

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : STARTUP, Entry : Multilink_PowerUpDelay, Value : 1000, R) => DI_OK

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : STARTUP, Entry : Multilink_PowerDownDelay, Value : 250, R) => DI_OK

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : STARTUP, Entry : FORCE_MASS_ERASE, Value : 0, R) => DI_OK

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : STARTUP, Entry : USE_SWD, Value : 1, R) => DI_OK

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : STARTUP, Entry : TraceLink_MaxBufferSize, Value : 1, R) => DI_OK

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : STARTUP, Entry : CPUTARGETTYPENAME, Value : HFSUIDFH5390FJIfnsdofnfjsdoiFHSIDO, R) => DI_ERR_NONFATAL

INF: P&E Interface detected - Flash Version 6.10

INF: Device is KL04Z8M4.

INF: Mode is In-Circuit Debug.

GDI: => DI_OK

GDI: DiMeeConnect(exec_env_id = 1)

GDI: => DI_OK

GDI: DiExecResetChild()

INF: CPU reset by debugger.

GDI: => DI_OK

GDI: DiExecGetStatus(cpu_status = (cause = GDI_WAIT_MISCELLANEOUS, brkpt_id = 0, reason = unknown state))

GDI: DiRegisterRead(PC (id:0xF))

GDI: => DI_OK

GDI: PC (id:0xF) -> 0x9F4

GDI: DiRegisterRead(SP (id:0xD))

GDI: => DI_OK

GDI: SP (id:0xD) -> 0x20000300

GDI: DiRegisterRead(LR (id:0xE))

GDI: => DI_OK

GDI: LR (id:0xE) -> 0xFFFFFFFF

Executing Initialization File: C:\Documents and Settings\Lab\workspace.10.4\KL04_Test/Project_Settings/Debugger/init_kinetis.tcl

radix x

cmdwin::eclipse::config hexprefix 0x

cmdwin::eclipse::config MemIdentifier p

cmdwin::eclipse::config MemWidth 32

cmdwin::eclipse::config MemAccess 32

GDI: DiRegisterRead(XPSR (id:0x10))

GDI: => DI_OK

GDI: XPSR (id:0x10) -> 0x21000000

GDI: DiMemoryRead(addr = 0x900, space = 4, mem_items = 64, size = 4)

cmdwin::eclipse::config MemSwap off

cmdwin::reg User\/System Mode Registers/LR = 0xFFFFFFFF

GDI: => DI_OK

GDI: FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF

GDI: FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF

GDI: FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF

GDI: FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF

GDI: FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF

GDI: FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF

GDI: FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF

GDI: FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF

GDI: DiMemoryRead(addr = 0xE000ED30, space = 4, mem_items = 1, size = 4)

GDI: => DI_OK

GDI: 0B 00 00 00

GDI: DiMemoryWrite(addr = 0xE000ED30, space = 4, mem_items = 1, size = 4)

GDI: 02 00 00 00

GDI: => DI_OK

GDI: DiRegisterWrite(LR (id:0xE), value = 0xFFFFFFFF)

GDI: => DI_OK

GDI: DiRegisterRead(LR (id:0xE))

GDI: => DI_OK

GDI: LR (id:0xE) -> 0xFFFFFFFF

GDI: DiRegisterRead(LR (id:0xE))

GDI: => DI_OK

GDI: LR (id:0xE) -> 0xFFFFFFFF

GDI: DiRegisterRead(SP (id:0xD))

GDI: => DI_OK

GDI: SP (id:0xD) -> 0x20000300

GDI: DiRegisterRead(LR (id:0xE))

GDI: => DI_OK

GDI: LR (id:0xE) -> 0xFFFFFFFF

thread break: Stopped, 0x0, 0x0, cpuARMLittle, KL04_Test.elf (state, tid, pid, cpu, target)

cmdwin::reg Breakpoint Unit Registers/BP_COMP0 = 0x0

GDI: DiMemoryWrite(addr = 0xE0002008, space = 4, mem_items = 1, size = 4)

GDI: 00 00 00 00

GDI: => DI_OK

cmdwin::reg Breakpoint Unit Registers/BP_COMP1 = 0x0

GDI: DiMemoryWrite(addr = 0xE000200C, space = 4, mem_items = 1, size = 4)

GDI: 00 00 00 00

GDI: => DI_OK

cmdwin::reg Core Debug Registers/DEMCR = 0x1000001

GDI: DiMemoryWrite(addr = 0xE000EDFC, space = 4, mem_items = 1, size = 4)

GDI: 01 00 00 01

GDI: => DI_OK

cmdwin::reg Data Watchpoint and Trace Unit Registers/DWT_FUNCTION0 = 0x0

GDI: DiMemoryWrite(addr = 0xE0001028, space = 4, mem_items = 1, size = 4)

GDI: 00 00 00 00

GDI: => DI_OK

cmdwin::reg Data Watchpoint and Trace Unit Registers/DWT_FUNCTION1 = 0x0

GDI: DiMemoryWrite(addr = 0xE0001038, space = 4, mem_items = 1, size = 4)

GDI: 00 00 00 00

GDI: => DI_OK

GDI: DiMemoryDownload(StartDownload)

GDI: => DI_OK

GDI: DiMemoryWrite(addr = 0x0, space = 4, mem_items = 48, size = 4)

GDI: 00 03 00 20 F5 09 00 00 95 05 00 00 A1 05 00 00 AD 05 00 00 B9 05 00 00 C5 05 00 00 D1 05 00 00

GDI: DD 05 00 00 E9 05 00 00 F5 05 00 00 01 06 00 00 0D 06 00 00 19 06 00 00 25 06 00 00 31 06 00 00

GDI: 3D 06 00 00 49 06 00 00 55 06 00 00 61 06 00 00 6D 06 00 00 79 06 00 00 85 06 00 00 91 06 00 00

GDI: 9D 06 00 00 A9 06 00 00 B5 06 00 00 C1 06 00 00 CD 06 00 00 D9 06 00 00 E5 06 00 00 F1 06 00 00

GDI: FD 06 00 00 09 07 00 00 15 07 00 00 21 07 00 00 2D 07 00 00 39 07 00 00 F1 04 00 00 45 07 00 00

GDI: 51 07 00 00 5D 07 00 00 69 07 00 00 75 07 00 00 81 07 00 00 8D 07 00 00 99 07 00 00 A5 07 00 00

GDI: => DI_OK

GDI: DiMemoryWrite(addr = 0x400, space = 4, mem_items = 4, size = 4)

GDI: FF FF FF FF FF FF FF FF FF FF FF FF 7E FF FF FF

GDI: => DI_OK

GDI: DiMemoryWrite(addr = 0x410, space = 4, mem_items = 526, size = 4)

GDI: 80 B5 84 B0 00 AF 78 60 2C 4B 1B 68 00 2B 43 D1 2B 4B FB 60 FB 68 7A 68 5A 60 FB 68 01 22 1A 70

GDI: 28 4B FA 68 1A 60 28 4A 27 49 28 4B CB 58 80 21 09 04 19 43 25 4B D1 50 25 4B 00 22 1A 60 24 4A

GDI: 84 23 5B 00 00 21 D1 50 21 4A 86 23 5B 00 01 21 D1 50 1F 4A 80 23 5B 00 1E 49 D1 50 1E 4A 1E 49

GDI: C5 23 9B 00 C9 58 1D 4B 0B 40 80 21 09 04 19 43 C5 23 9B 00 D1 50 18 4B 17 4A 12 68 80 21 C9 03

GDI: 0A 43 1A 60 12 4A 84 23 5B 00 03 21 D1 50 0B 4B FA 68 1A 60 FB 68 0C E0 08 4B 1B 68 FB 60 FB 68

GDI: 7A 68 5A 60 FB 68 1B 78 01 33 DA B2 FB 68 1A 70 FB 68 18 1C BD 46 04 B0 80 BD C0 46 18 FE FF 1F

GDI: 00 FE FF 1F 08 FE FF 1F 00 70 04 40 3C 10 00 00 00 70 03 40 FF FF 9F 00 00 E1 00 E0 FF FF 00 FF

GDI: 80 B5 82 B0 00 AF 0A 4B 1B 68 7B 60 09 4A 86 23 5B 00 01 21 D1 50 07 4A 80 23 5B 00 D3 58 7B 68

GDI: 5B 68 18 1C 00 F0 2C F8 BD 46 02 B0 80 BD C0 46 08 FE FF 1F 00 70 03 40 80 B5 84 B0 00 AF 78 60

GDI: 0D 4B FB 60 FB 68 7A 68 9A 60 FB 68 01 22 1A 71 00 20 FF F7 65 FF 02 1C FB 68 1A 60 FB 68 1B 68

GDI: 00 2B 01 D1 00 23 03 E0 04 4B FA 68 5A 60 FB 68 18 1C BD 46 04 B0 80 BD 0C FE FF 1F 18 FE FF 1F

GDI: 80 B5 84 B0 00 AF 78 60 05 4B 5B 68 FB 60 FB 68 9B 68 18 1C 00 F0 5A FA BD 46 04 B0 80 BD C0 46

GDI: 18 FE FF 1F 80 B5 00 AF FF BE BD 46 80 BD C0 46 80 B5 00 AF FF BE BD 46 80 BD C0 46 80 B5 00 AF

GDI: FF BE BD 46 80 BD C0 46 80 B5 00 AF FF BE BD 46 80 BD C0 46 80 B5 00 AF FF BE BD 46 80 BD C0 46

GDI: 80 B5 00 AF FF BE BD 46 80 BD C0 46 80 B5 00 AF FF BE BD 46 80 BD C0 46 80 B5 00 AF FF BE BD 46

GDI: 80 BD C0 46 80 B5 00 AF FF BE BD 46 80 BD C0 46 80 B5 00 AF FF BE BD 46 80 BD C0 46 80 B5 00 AF

GDI: FF BE BD 46 80 BD C0 46 80 B5 00 AF FF BE BD 46 80 BD C0 46 80 B5 00 AF FF BE BD 46 80 BD C0 46

GDI: 80 B5 00 AF FF BE BD 46 80 BD C0 46 80 B5 00 AF FF BE BD 46 80 BD C0 46 80 B5 00 AF FF BE BD 46

GDI: 80 BD C0 46 80 B5 00 AF FF BE BD 46 80 BD C0 46 80 B5 00 AF FF BE BD 46 80 BD C0 46 80 B5 00 AF

GDI: FF BE BD 46 80 BD C0 46 80 B5 00 AF FF BE BD 46 80 BD C0 46 80 B5 00 AF FF BE BD 46 80 BD C0 46

GDI: 80 B5 00 AF FF BE BD 46 80 BD C0 46 80 B5 00 AF FF BE BD 46 80 BD C0 46 80 B5 00 AF FF BE BD 46

GDI: 80 BD C0 46 80 B5 00 AF FF BE BD 46 80 BD C0 46 80 B5 00 AF FF BE BD 46 80 BD C0 46 80 B5 00 AF

GDI: FF BE BD 46 80 BD C0 46 80 B5 00 AF FF BE BD 46 80 BD C0 46 80 B5 00 AF FF BE BD 46 80 BD C0 46

GDI: 80 B5 00 AF FF BE BD 46 80 BD C0 46 80 B5 00 AF FF BE BD 46 80 BD C0 46 80 B5 00 AF FF BE BD 46

GDI: 80 BD C0 46 80 B5 00 AF FF BE BD 46 80 BD C0 46 80 B5 00 AF FF BE BD 46 80 BD C0 46 80 B5 00 AF

GDI: FF BE BD 46 80 BD C0 46 80 B5 00 AF FF BE BD 46 80 BD C0 46 80 B5 00 AF FF BE BD 46 80 BD C0 46

GDI: 80 B5 00 AF FF BE BD 46 80 BD C0 46 80 B5 00 AF FF BE BD 46 80 BD C0 46 80 B5 00 AF FF BE BD 46

GDI: 80 BD C0 46 80 B5 00 AF FF BE BD 46 80 BD C0 46 80 B5 00 AF FF BE BD 46 80 BD C0 46 80 B5 00 AF

GDI: FF BE BD 46 80 BD C0 46 80 B5 00 AF FF BE BD 46 80 BD C0 46 80 B5 00 AF FF BE BD 46 80 BD C0 46

GDI: 80 B5 00 AF 25 4A 26 49 26 4B D1 50 26 4A 88 23 5B 01 00 21 D1 50 24 4A 23 49 24 4B CB 58 C0 21

GDI: C9 00 19 43 21 4B D1 50 1F 4A 21 4B 00 21 D1 50 1D 4B 1D 4A 12 68 C0 21 09 03 0A 43 1A 60 1A 4A

GDI: 19 49 1C 4B C9 58 1C 4B 0B 40 80 21 49 04 19 43 18 4B D1 50 19 4B 06 22 1A 70 18 4B 00 22 5A 70

GDI: 16 4B 16 4A D2 78 D1 B2 1F 22 0A 40 D2 B2 DA 70 13 4B 80 22 1A 70 C0 46 10 4B 9B 79 DB B2 1A 1C

GDI: 10 23 13 40 F8 D0 C0 46 0C 4B 9B 79 DB B2 1A 1C 0C 23 13 40 F8 D1 BD 46 80 BD C0 46 00 E0 00 E0

GDI: 00 00 00 00 08 0D 00 00 00 70 04 40 38 10 00 00 44 10 00 00 04 10 00 00 FF FF FF FC 00 40 06 40

GDI: 00 50 06 40 80 B5 00 AF 2C 4B 2C 4A 51 69 2C 4A 0A 40 C0 21 89 00 0A 43 5A 61 2A 4B 29 4A 52 79

GDI: D2 B2 1F 21 8A 43 D2 B2 5A 71 26 4B 25 4A 12 79 D2 B2 07 21 8A 43 D2 B2 1A 71 23 4B 22 4A 12 78

GDI: D2 B2 D2 B2 73 21 8A 43 D2 B2 50 21 0A 43 D2 B2 D2 B2 1A 70 1C 4B 1C 4A 52 78 D2 B2 D2 B2 63 21

GDI: 8A 43 D2 B2 40 21 0A 43 D2 B2 D2 B2 5A 70 16 4B 15 4A 92 78 D2 B2 19 21 8A 43 D2 B2 9A 70 13 4B

GDI: 00 22 1A 70 12 4B 12 4A 51 68 0D 4A 0A 40 C0 21 89 00 0A 43 5A 60 0F 4A 0E 49 C1 23 9B 00 C9 58

GDI: 0D 4B 19 40 C1 23 9B 00 D1 50 00 20 FF F7 04 FE 00 20 00 F0 13 F8 62 B6 BD 46 80 BD 00 A0 04 40

GDI: FF F8 FF FE 00 F0 07 40 00 D0 07 40 00 E0 07 40 00 90 04 40 00 E1 00 E0 FF FF 00 FF 80 B5 84 B0

GDI: 00 AF 78 60 11 4B FB 60 FB 68 7A 68 1A 60 10 4B 0F 4A 52 69 80 21 49 00 0A 43 5A 61 0C 4B 0C 4A

GDI: 11 68 0C 4A 0A 40 1A 60 0B 4B 0B 4A 11 6A 0B 4A 0A 40 80 21 49 00 0A 43 1A 62 09 4B FA 68 9A 60

GDI: FB 68 18 1C BD 46 04 B0 80 BD C0 46 24 FE FF 1F 40 F0 0F 40 FF FE FF FF 00 A0 04 40 FF F8 FF FE

GDI: 18 FE FF 1F 80 B5 82 B0 00 AF 78 60 03 4B 80 22 52 00 DA 60 BD 46 02 B0 80 BD C0 46 40 F0 0F F8

GDI: 80 B5 00 AF 05 4A 06 4B D3 1A 05 4A 10 1C 00 21 1A 1C 00 F0 51 F8 BD 46 80 BD C0 46 44 FE FF 1F

GDI: 00 FE FF 1F 00 F0 18 F9 FF F7 DA FE FF F7 E8 FF 00 F0 EA F8 00 F0 86 F8 00 F0 1C F9 04 4B 00 20

GDI: 19 1C 00 F0 0D F8 03 1C 18 1C 00 F0 19 F8 C0 46 28 FE FF 1F 80 B5 82 B0 00 AF 78 60 FE E7 C0 46

GDI: 80 B5 00 AF FF F7 1E FF FE E7 C0 46 80 B5 82 B0 00 AF 78 60 00 20 FF F7 B5 FF BD 46 02 B0 80 BD

GDI: 38 B5 05 1C 00 F0 DA F8 00 F0 80 F8 08 4C 23 68 00 2B 02 D0 98 47 00 20 20 60 06 4C 21 68 00 29

GDI: 02 D0 88 47 00 22 22 60 28 1C FF F7 D3 FF 38 BD 2C FE FF 1F 30 FE FF 1F 10 B5 04 1C 00 F0 02 F8

GDI: 20 1C 10 BD 30 B5 C9 B2 03 1C 1F 2A 31 D9 44 42 03 23 23 40 05 D0 D2 1A C5 18 01 70 01 30 A8 42

GDI: FB D1 00 29 05 D0 0D 06 0C 04 2C 43 0B 02 21 43 19 43 54 09 03 1C 00 2C 0E D0 25 1C 01 3D 19 60

GDI: 59 60 99 60 D9 60 19 61 59 61 99 61 D9 61 20 33 00 2D F3 D1 63 01 C3 18 D0 06 40 0F 07 D0 04 1C

GDI: 1D 1C 01 3C 02 C5 00 2C FB D1 80 00 1B 18 03 24 22 40 9D 18 00 2A 03 D0 19 70 01 33 AB 42 FB D1

GDI: 30 BD 00 00 10 B5 0B 4C 0B 4B 9C 42 02 D0 01 CC 80 47 F9 E7 09 4C 0A 48 84 42 02 D0 08 CC 98 47

GDI: F9 E7 08 4C 08 49 8C 42 02 D0 04 CC 90 47 F9 E7 10 BD C0 46 48 0C 00 00 48 0C 00 00 48 0C 00 00

GDI: 48 0C 00 00 48 0C 00 00 48 0C 00 00 10 B5 08 4C 08 4B 9C 42 02 D0 04 CC 90 47 F9 E7 06 4C 07 48

GDI: 84 42 03 D0 04 3C 21 68 88 47 F8 E7 10 BD C0 46 48 0C 00 00 48 0C 00 00 48 0C 00 00 48 0C 00 00

GDI: 00 B5 88 42 1F D0 00 2A 1D D0 03 23 19 42 07 D1 18 42 05 D1 9A 42 03 D9 08 C9 04 3A 08 C0 F2 E7

GDI: 01 23 19 42 09 D1 18 42 07 D1 9A 42 05 D9 0B 88 02 3A 03 80 02 31 02 30 E5 E7 0B 78 01 3A 03 70

GDI: 01 31 01 30 DF E7 00 BD 38 B5 0B 4D 00 2D 11 D0 00 24 2B 19 19 68 00 29 06 D0 2B 19 58 68 9A 68

GDI: FF F7 CE FF 0C 34 F4 E7 5A 68 00 2A F5 D1 98 68 00 28 F2 D1 38 BD C0 46 48 0C 00 00 05 4B 10 B5

GDI: 1C 68 00 2C 04 D0 A0 68 61 68 88 47 24 68 F8 E7 10 BD C0 46 40 FE FF 1F 05 4B 18 1C 00 28 05 D0

GDI: 85 46 81 B0 00 20 C0 43 00 90 01 B0 F7 46 70 47 00 03 00 20 F7 46 70 47

GDI: => DI_OK

GDI: DiMemoryWrite(addr = 0xC48, space = 4, mem_items = 6, size = 4)

GDI: 48 0C 00 00 00 FE FF 1F 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

GDI: => DI_OK

GDI: DiMemoryDownload(EndDownload)

Starting 3rd party flash programming...

GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : STARTUP, Entry : SPECIFY_NETWORKCARD_ENABLED, Value : 0, R) => DI_OK

INF: Copyright 2012 P&E Microcomputer Systems,Inc.

INF: Command Line :"C:\Freescale\CW MCU v10.4\eclipse\..\MCU\bin\de.exe" -noni -language en -ORBendPoint giop:tcp:127.0.0.1: -ORBtraceLevel 0

INF: CMD>RE

INF: Initializing.

INF: Target has been RESET and is active.

INF: CMD>CM C:\Freescale\CW MCU v10.4\MCU\bin\Plugins\support\arm\gdi\P&E\freescale_kl04z8m4_1x32x2k_pflash.arp

INF: Initializing.

INF:  Frequency ~ 20971785

INF: (Recommended TRIM=$0089,FTRIM=1)

INF: Initialized.

INF: ;version 1.01, 03/14/2013, Copyright P&E Microcomputer Systems, www.pemicro.com [mk_8k_n_pflash_m0]

INF: ;device freescale, kl04z8m4, 1x32x2k, desc=pflash

INF: ;begin_cs device=$00000000, length=$00002000, ram=$20000000

INF: Loading programming algorithm ...

INF: Done.

INF: CMD>EM

INF: Erasing.

INF: Module has been erased.

INF: Initializing.

INF: Initialized.

INF: ;version 1.01, 03/14/2013, Copyright P&E Microcomputer Systems, www.pemicro.com [mk_8k_n_pflash_m0]

INF: ;device freescale, kl04z8m4, 1x32x2k, desc=pflash

INF: ;begin_cs device=$00000000, length=$00002000, ram=$20000000

INF: Loading programming algorithm ...

INF: Done.

INF: CMD>PM

INF: Programming.

INF: Processing Object File Data ...

INF: Error during programming.

ERR: Error Programming flash of device

ERR: Error occured during Flash programming.

GDI: => DI_OK

GDI: DiMemoryRead(addr = 0x0, space = 4, mem_items = 48, size = 4)

GDI: => DI_OK

GDI: 00 03 00 20 F5 09 00 00 95 05 00 00 A1 05 00 00 AD 05 00 00 B9 05 00 00 C5 05 00 00 D1 05 00 00

GDI: DD 05 00 00 E9 05 00 00 F5 05 00 00 01 06 00 00 0D 06 00 00 19 06 00 00 25 06 00 00 31 06 00 00

GDI: 3D 06 00 00 49 06 00 00 55 06 00 00 61 06 00 00 6D 06 00 00 79 06 00 00 85 06 00 00 91 06 00 00

GDI: 9D 06 00 00 A9 06 00 00 B5 06 00 00 C1 06 00 00 CD 06 00 00 D9 06 00 00 E5 06 00 00 F1 06 00 00

GDI: FD 06 00 00 09 07 00 00 15 07 00 00 21 07 00 00 2D 07 00 00 39 07 00 00 F1 04 00 00 45 07 00 00

GDI: 51 07 00 00 5D 07 00 00 69 07 00 00 75 07 00 00 81 07 00 00 8D 07 00 00 99 07 00 00 A5 07 00 00

GDI: DiMemoryRead(addr = 0x400, space = 4, mem_items = 4, size = 4)

GDI: => DI_OK

GDI: FF FF FF FF FF FF FF FF FF FF FF FF 7E FF FF FF

GDI: DiMemoryRead(addr = 0x410, space = 4, mem_items = 526, size = 4)

GDI: => DI_OK

GDI: 80 B5 84 B0 00 AF 78 60 2C 4B 1B 68 00 2B 43 D1 2B 4B FB 60 FB 68 7A 68 5A 60 FB 68 01 22 1A 70

GDI: 28 4B FA 68 1A 60 28 4A 27 49 28 4B CB 58 80 21 09 04 19 43 25 4B D1 50 25 4B 00 22 1A 60 24 4A

GDI: 84 23 5B 00 00 21 D1 50 21 4A 86 23 5B 00 01 21 D1 50 1F 4A 80 23 5B 00 1E 49 D1 50 1E 4A 1E 49

GDI: C5 23 9B 00 C9 58 1D 4B 0B 40 80 21 09 04 19 43 C5 23 9B 00 D1 50 18 4B 17 4A 12 68 80 21 C9 03

GDI: 0A 43 1A 60 12 4A 84 23 5B 00 03 21 D1 50 0B 4B FA 68 1A 60 FB 68 0C E0 08 4B 1B 68 FB 60 FB 68

GDI: 7A 68 5A 60 FB 68 1B 78 01 33 DA B2 FB 68 1A 70 FB 68 18 1C BD 46 04 B0 80 BD C0 46 18 FE FF 1F

GDI: 00 FE FF 1F 08 FE FF 1F 00 70 04 40 3C 10 00 00 00 70 03 40 FF FF 9F 00 00 E1 00 E0 FF FF 00 FF

GDI: 80 B5 82 B0 00 AF 0A 4B 1B 68 7B 60 09 4A 86 23 5B 00 01 21 D1 50 07 4A 80 23 5B 00 D3 58 7B 68

GDI: 5B 68 18 1C 00 F0 2C F8 BD 46 02 B0 80 BD C0 46 08 FE FF 1F 00 70 03 40 80 B5 84 B0 00 AF 78 60

GDI: 0D 4B FB 60 FB 68 7A 68 9A 60 FB 68 01 22 1A 71 00 20 FF F7 65 FF 02 1C FB 68 1A 60 FB 68 1B 68

GDI: 00 2B 01 D1 00 23 03 E0 04 4B FA 68 5A 60 FB 68 18 1C BD 46 04 B0 80 BD 0C FE FF 1F 18 FE FF 1F

GDI: 80 B5 84 B0 00 AF 78 60 05 4B 5B 68 FB 60 FB 68 9B 68 18 1C 00 F0 5A FA BD 46 04 B0 80 BD C0 46

GDI: 18 FE FF 1F 80 B5 00 AF FF BE BD 46 80 BD C0 46 80 B5 00 AF FF BE BD 46 80 BD C0 46 80 B5 00 AF

GDI: FF BE BD 46 80 BD C0 46 80 B5 00 AF FF BE BD 46 80 BD C0 46 80 B5 00 AF FF BE BD 46 80 BD C0 46

GDI: 80 B5 00 AF FF BE BD 46 80 BD C0 46 80 B5 00 AF FF BE BD 46 80 BD C0 46 80 B5 00 AF FF BE BD 46

GDI: 80 BD C0 46 FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF

GDI: FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF

GDI: FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF

GDI: FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF

GDI: FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF

GDI: FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF

GDI: FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF

GDI: FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF

GDI: FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF

GDI: FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF

GDI: FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF

GDI: FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF

GDI: FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF

GDI: FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF

GDI: FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF

GDI: FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF

GDI: FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF

GDI: FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF

GDI: FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF

GDI: FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF

GDI: FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF

GDI: FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF

GDI: FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF

GDI: FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF

GDI: FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF

GDI: FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF

GDI: FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF

GDI: FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF

GDI: FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF

GDI: FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF

GDI: FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF

GDI: FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF

GDI: FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF

GDI: FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF

GDI: FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF

GDI: FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF

GDI: FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF

GDI: FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF

GDI: FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF

GDI: FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF

GDI: FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF

GDI: FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF

GDI: FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF

GDI: FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF

GDI: FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF

GDI: FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF

GDI: FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF

GDI: FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF

GDI: FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF

GDI: FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF

GDI: FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF


0 项奖励
回复
5,080 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Joe,

Seems only part of the codes have been downloaded successfully, I will check it with the CW team and let you know when I have any more information.

BTW, would you please show me the debugger configuration that you are using? just like below:

1.PNG

Thanks for your patience!!

B.R

Kan

0 项奖励
回复
5,080 次查看
joevignola
Contributor III

Here is my configuration

KL04_debug.PNG

0 项奖励
回复
5,080 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Joe,

Thanks for the information!! I have just discussed with the CW support team, and they would like to ask for more information during the programming, would you please check the option shown as below? That might help to give more information regarding this issue.

prg_dialog.JPG

BTW, do you have another board with KL04Z? is it the same result?

Thanks for your patience!!

B.R

Kan

0 项奖励
回复
5,080 次查看
joevignola
Contributor III

Here is the dialog that pops up.

PandEMicro.JPG

0 项奖励
回复
5,080 次查看
joevignola
Contributor III

Here is the basic schematic that I'm using.

Joe.

KL04_basic.png

0 项奖励
回复
5,080 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Thanks for the information!! The schematics should be ok, but it still hard to locate the possible cause. Have you got another programmer such as Jlink to have a try? if not, I remember you have a FRDM-KL05Z , and its on board OpenSDA can be used to program the external device, would you please try it following the guide from Debug External Processors with USBDM and Freedom Board | MCU on Eclipse?

Please kindly let me know if the problem is still there.

B.R

Kan