MK70FN1M0 Micro controller reboots frequently

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MK70FN1M0 Micro controller reboots frequently

3,225 Views
marlinx
Contributor II

Hi

I am using MK70FN1M0 Micro controller on one of my Board.

Issue i am facing is my MK70FN1M0 board frequently reboots. i can say after every 1 to 2 mins board reboots(time is not fixed it varies).

What could be the issue?? which is causing board to reboot frequently.

Please anybody can give suggestion to solve this issue, ASAP.

Regards

Marlin

6 Replies

3,051 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello ,

Please change a USB line to test .

BR

Alice

0 Kudos
Reply

3,051 Views
marlinx
Contributor II

thanks for the quick reply Alice.

Can you Please elaborate "change a USB line to test".

Marlinx

0 Kudos
Reply

3,051 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello ,

I recommend you firstly finding out  the reason is software or hardware, so please do like this :

1) create a simple project ,then test it , if it can work well , the problem is your software.

2) it the simple project still make the board reboot , it maybe your board design reason , please check the circuit , maybe the watchdog , maybe some disturb made the mcu reset.

This need analysis your board circuit seriously .

Best Regards,

Alice

------------------------------------------------------------------------------------------

If this post answers your question, please click the Correct Answer button.

-----------------------------------------------------------------------------------

If this post help your question, please click the helpful Answer button.

0 Kudos
Reply

3,051 Views
marlinx
Contributor II

Hi Alice,

thanks for the Reply.

the problem is associated with our designed board, Not with demo board.

One more thing i want bring in to your notice that i have couple of MK70FN1M0 boards. Some boards are working without any issues i.e. without any reboot issues.

in some of the boards i am facing this rebooting issue.

even i am thinking the problem is with hardware or software, difficult to figure out!!!

at outer level i think some event is causing reset again and again which is causing system to reboot again and again. first i need to figure out which is source of reset.

Regards

Marlin

0 Kudos
Reply

3,051 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Marlinx,

The rebooting issue is difficult to track, software/hardware both can cause the issue,  I am not sure I can solve it.

But i think you can check the RESET status register to know the cause of the rebooting. Pls check the RCM_SRS0 and RCM_SRS1 registers after the rebooting happens, or you can output the two register via Rs232 so that you can know the register when the chip is running.

Pls refer to section 13.2.2 System Reset Status Register 1 (RCM_SRS1) in  reference manual of K70 for the bit mapping in the register.

hope it can give a clue.

BR

XiangJun Rong

3,051 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello ,

Does your board made by yourself , or is the demo board of freesacle TWR-K70 ?

If it is the TWR-K70 of freescale , please update the firmware .

If it is not , there will be some hardware engineer give your some suggestion.

Best Regards,

Alice

------------------------------------------------------------------------------------------

If this post answers your question, please click the Correct Answer button.

-----------------------------------------------------------------------------------

If this post help your question, please click the helpful Answer button.

0 Kudos
Reply