MK64 : Is Program flash 0 IFR map modified by " Program Partition command "

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MK64 : Is Program flash 0 IFR map modified by " Program Partition command "

跳至解决方案
1,830 次查看
koichisakagami
Contributor II

Dear community,
       I am checking a MK64FX512VLL12 behavior .

After issuing the " Program Partition command ",
Is the Program flash 0 IFR map content changed ?

As far as I was confirmed, the content had not changed.

Best Regards,

       Koichi Sakagami

标签 (1)
0 项奖励
回复
1 解答
1,619 次查看
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi

The K64 product Flash with FlexNVM has program flash and data flash.

The " Program Partition command " will modify the [EEPROM Data Set Size] & [FlexNVM Partition Code] at Data flash 0 IFR.

The program flash 0 IFR value will not be affected.


Wish it helps.

Have a great day,
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,620 次查看
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi

The K64 product Flash with FlexNVM has program flash and data flash.

The " Program Partition command " will modify the [EEPROM Data Set Size] & [FlexNVM Partition Code] at Data flash 0 IFR.

The program flash 0 IFR value will not be affected.


Wish it helps.

Have a great day,
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复