MK64 : Is Program flash 0 IFR map modified by " Program Partition command "

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MK64 : Is Program flash 0 IFR map modified by " Program Partition command "

ソリューションへジャンプ
1,848件の閲覧回数
koichisakagami
Contributor II

Dear community,
       I am checking a MK64FX512VLL12 behavior .

After issuing the " Program Partition command ",
Is the Program flash 0 IFR map content changed ?

As far as I was confirmed, the content had not changed.

Best Regards,

       Koichi Sakagami

ラベル(1)
0 件の賞賛
返信
1 解決策
1,637件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi

The K64 product Flash with FlexNVM has program flash and data flash.

The " Program Partition command " will modify the [EEPROM Data Set Size] & [FlexNVM Partition Code] at Data flash 0 IFR.

The program flash 0 IFR value will not be affected.


Wish it helps.

Have a great day,
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,638件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi

The K64 product Flash with FlexNVM has program flash and data flash.

The " Program Partition command " will modify the [EEPROM Data Set Size] & [FlexNVM Partition Code] at Data flash 0 IFR.

The program flash 0 IFR value will not be affected.


Wish it helps.

Have a great day,
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信