MK64 : Is Program flash 0 IFR map modified by " Program Partition command "

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MK64 : Is Program flash 0 IFR map modified by " Program Partition command "

Jump to solution
1,851 Views
koichisakagami
Contributor II

Dear community,
       I am checking a MK64FX512VLL12 behavior .

After issuing the " Program Partition command ",
Is the Program flash 0 IFR map content changed ?

As far as I was confirmed, the content had not changed.

Best Regards,

       Koichi Sakagami

Labels (1)
0 Kudos
Reply
1 Solution
1,640 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi

The K64 product Flash with FlexNVM has program flash and data flash.

The " Program Partition command " will modify the [EEPROM Data Set Size] & [FlexNVM Partition Code] at Data flash 0 IFR.

The program flash 0 IFR value will not be affected.


Wish it helps.

Have a great day,
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,641 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi

The K64 product Flash with FlexNVM has program flash and data flash.

The " Program Partition command " will modify the [EEPROM Data Set Size] & [FlexNVM Partition Code] at Data flash 0 IFR.

The program flash 0 IFR value will not be affected.


Wish it helps.

Have a great day,
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply