MK60DN512VLQ10 4N30D flash program section command still not working?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MK60DN512VLQ10 4N30D flash program section command still not working?

2,216 次查看
comsosysarch
Contributor III

Freescale indicates the issue with the MK60DN512VLQ10 flash program section (PGMSEC, 0x0b) command (it would actually be rejected on 2N30D v1.2 silicon) has been fixed on 4N30D v1.4 silicon.

 

On the v1.4 devices I am working with I am still having trouble with this command. Mind you I had no problems with the same code on v1.0. The problem now is not that the command is rejected, but rather the command never completes and the processor remain stuck in an endless loop waiting for the FTFL FSTAT register CCIF bit. This has been on multiple devices and I have not seen any actually work yet.

 

I guess what I am asking is if anyone else has had this issue or do I just have a code bug or maybe a bad batch of chips?

 

To that end, here is my flash writing code (always called after a successful erase)...

 

bool ftflPgmSec(UInt32 flAddr, UInt16 num64s)
{
    if(flAddr & 0xff000007)
        return false;
    if(num64s == 0)
        return false;
    if(flAddr < 0x00040000 || flAddr > 0x0007ffff)
        return false;
#ifdef SI_2N30D_PGMSEC_PROBLEM {  UInt32 subWrAddr, subRdAddr;  for(subWrAddr = flAddr, subRdAddr = 0x14000000; subWrAddr < flAddr + 8 * num64s; subWrAddr += 4, subRdAddr += 4)  {   while(!(FTFL_BASE_PTR->FSTAT & FTFL_FSTAT_CCIF_MASK)); // wait for any previous command to complete (required to proceed)   if(FTFL_BASE_PTR->FSTAT & (FTFL_FSTAT_ACCERR_MASK | FTFL_FSTAT_FPVIOL_MASK)) // check for previous command error flags    FTFL_BASE_PTR->FSTAT = (FTFL_FSTAT_ACCERR_MASK | FTFL_FSTAT_FPVIOL_MASK); // write 1 to clear error flags (required to proceed)   FTFL_BASE_PTR->FCCOB0 = 0x06; // program longword command   FTFL_BASE_PTR->FCCOB1 = (UInt08)((subWrAddr & 0x00ff0000) >> 16);   FTFL_BASE_PTR->FCCOB2 = (UInt08)((subWrAddr & 0x0000ff00) >> 8);   FTFL_BASE_PTR->FCCOB3 = (UInt08)(subWrAddr & 0x000000fc);   FTFL_BASE_PTR->FCCOB4 = *((UInt08 *)subRdAddr + 3);   FTFL_BASE_PTR->FCCOB5 = *((UInt08 *)subRdAddr + 2);   FTFL_BASE_PTR->FCCOB6 = *((UInt08 *)subRdAddr + 1);   FTFL_BASE_PTR->FCCOB7 = *((UInt08 *)subRdAddr + 0);   FTFL_BASE_PTR->FSTAT = FTFL_FSTAT_CCIF_MASK; // write 1 to clear flag (executes command)   while(!(FTFL_BASE_PTR->FSTAT & FTFL_FSTAT_CCIF_MASK)); // wait for command to complete   if(FTFL_BASE_PTR->FSTAT & (FTFL_FSTAT_ACCERR_MASK | FTFL_FSTAT_FPVIOL_MASK | FTFL_FSTAT_MGSTAT0_MASK)) return false; // return command error flag status  }  return true; }#else while(!(FTFL_BASE_PTR->FSTAT & FTFL_FSTAT_CCIF_MASK)); // wait for any previous command to complete (required to proceed) if(FTFL_BASE_PTR->FSTAT & (FTFL_FSTAT_ACCERR_MASK | FTFL_FSTAT_FPVIOL_MASK)) // check for previous command error flags  FTFL_BASE_PTR->FSTAT = (FTFL_FSTAT_ACCERR_MASK | FTFL_FSTAT_FPVIOL_MASK); // write 1 to clear error flags (required to proceed) FTFL_BASE_PTR->FCCOB0 = 0x0b; // program section command FTFL_BASE_PTR->FCCOB1 = (UInt08)((flAddr & 0x00ff0000) >> 16); FTFL_BASE_PTR->FCCOB2 = (UInt08)((flAddr & 0x0000ff00) >> 8); FTFL_BASE_PTR->FCCOB3 = (UInt08)(flAddr & 0x000000f8); FTFL_BASE_PTR->FCCOB4 = (UInt08)(num64s >> 8); FTFL_BASE_PTR->FCCOB5 = (UInt08)(num64s & 0x00ff); FTFL_BASE_PTR->FSTAT = FTFL_FSTAT_CCIF_MASK; // write 1 to clear flag (executes command) while(!(FTFL_BASE_PTR->FSTAT & FTFL_FSTAT_CCIF_MASK)); // wait for command to complete return((FTFL_BASE_PTR->FSTAT & (FTFL_FSTAT_ACCERR_MASK | FTFL_FSTAT_FPVIOL_MASK | FTFL_FSTAT_MGSTAT0_MASK)) == 0); // return command error flag status#endif
}

 

0 项奖励
回复
2 回复数

1,846 次查看
Klayton
Contributor III

I am having similar issues on some 4N30D version K10 parts.  When erasing or writing flash it gets hung waiting on the CCIF to be cleared.  Have asked my Freescale rep for help on this and so far have heard nothing.

0 项奖励
回复

1,846 次查看
comsosysarch
Contributor III

If you could not guess, after the successful flash erasure the data to be written was placed in the flash acceleration buffer at 0x14000000 prior to calling this function (which just executes the FTFL command to write some number of 64-bit phrases of that data).

 

SI_2N30D_PGMSEC_PROBLEM gets defined for the buggy v1.2 silicon where the PGMSEC command did not work and was rejected. For v1.4 I had been hoping I could go back to using the PGMSEC command but as described I have not had any luck with it.

 

The original without the #define did work on v1.0 silicon and the version with the #define did work on v1.2 and v1.4 silicon.

 

But on v1.4 when I remove the #define and run the resulting code it hangs waiting for the CCIF bit to indicate command completion.

 

The only thing I have heard from asking Freescale is that as far as they know this should work on v1.4 chips.

0 项奖励
回复