MK60DN512VLL10 header file no SRSL for reset cause

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MK60DN512VLL10 header file no SRSL for reset cause

跳至解决方案
1,239 次查看
CiaranMacA_hkc
Contributor III

The latest version of my header for this part "MK60D10.h" does not seem to have access to reset cause register SRSL. Indeed the same for the RM. For other versions of the K series you can read reset cause from SRSL.

Extract from header version:

** Reference manual:K60P144M100SF2V2RM Rev. 2, Jun 2012
** Version:         rev. 1.8, 2013-06-24

I need to read back the reset cause. Any ideas?

Thanks

Ciarán Mac Aonghusa.

0 项奖励
回复
1 解答
1,107 次查看
perlam_i_au
Senior Contributor I

The System Register Status is defined in the header file as SRS0 and SRS1, check it out so you can correct your code and let me know if I can help you with something else.:smileyhappy:

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,108 次查看
perlam_i_au
Senior Contributor I

The System Register Status is defined in the header file as SRS0 and SRS1, check it out so you can correct your code and let me know if I can help you with something else.:smileyhappy:

0 项奖励
回复
1,107 次查看
CiaranMacA_hkc
Contributor III

Thank you Perla Andrea.

0 项奖励
回复