MK60DN512VLL10 header file no SRSL for reset cause

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MK60DN512VLL10 header file no SRSL for reset cause

ソリューションへジャンプ
1,281件の閲覧回数
CiaranMacA_hkc
Contributor III

The latest version of my header for this part "MK60D10.h" does not seem to have access to reset cause register SRSL. Indeed the same for the RM. For other versions of the K series you can read reset cause from SRSL.

Extract from header version:

** Reference manual:K60P144M100SF2V2RM Rev. 2, Jun 2012
** Version:         rev. 1.8, 2013-06-24

I need to read back the reset cause. Any ideas?

Thanks

Ciarán Mac Aonghusa.

0 件の賞賛
返信
1 解決策
1,149件の閲覧回数
perlam_i_au
Senior Contributor I

The System Register Status is defined in the header file as SRS0 and SRS1, check it out so you can correct your code and let me know if I can help you with something else.:smileyhappy:

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,150件の閲覧回数
perlam_i_au
Senior Contributor I

The System Register Status is defined in the header file as SRS0 and SRS1, check it out so you can correct your code and let me know if I can help you with something else.:smileyhappy:

0 件の賞賛
返信
1,149件の閲覧回数
CiaranMacA_hkc
Contributor III

Thank you Perla Andrea.

0 件の賞賛
返信