MK50DN512CMC10

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MK50DN512CMC10

Jump to solution
1,392 Views
damonkutten
Contributor II

I have a question about memory on the MK50DN512CMC10. Does this device contain any non-volatile storage,

that can be used by the program (running out of program flash) to store a few hundred bytes of data, for example unique serial numbers and configuration information? I am a bit confused by the documentation. In the K50 Sub-Family Reference Manual, there is a table on page 99 (Section 3.5.1.2) that shows 4KB of FlexRAM in this device, but it has no FlexNVM. What storage resources are actually available?

Thanks.

0 Kudos
Reply
1 Solution
1,281 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Damon,

    1. non volatile storage

        Please go to page 636,  Program Flash IFR Map, there just has 64 program once field.

      If you want to use the unique serial number, the K50 has the Unique Identification Register, it contains the chip UID.

  2. FlexRAM

      You can find just MK50DX256CMC10 has the flexNVM and the FlexRAM, your chip is MK50DN512CMC10, it just has the Program flash.

  So, if the 64bits IFR is not enough, you may use the flash to store your configuration information.

Wish it helps you!


Have a great day,
Jingjing

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,282 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Damon,

    1. non volatile storage

        Please go to page 636,  Program Flash IFR Map, there just has 64 program once field.

      If you want to use the unique serial number, the K50 has the Unique Identification Register, it contains the chip UID.

  2. FlexRAM

      You can find just MK50DX256CMC10 has the flexNVM and the FlexRAM, your chip is MK50DN512CMC10, it just has the Program flash.

  So, if the 64bits IFR is not enough, you may use the flash to store your configuration information.

Wish it helps you!


Have a great day,
Jingjing

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply