MK50DN512CMC10

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,497件の閲覧回数
damonkutten
Contributor II

I have a question about memory on the MK50DN512CMC10. Does this device contain any non-volatile storage,

that can be used by the program (running out of program flash) to store a few hundred bytes of data, for example unique serial numbers and configuration information? I am a bit confused by the documentation. In the K50 Sub-Family Reference Manual, there is a table on page 99 (Section 3.5.1.2) that shows 4KB of FlexRAM in this device, but it has no FlexNVM. What storage resources are actually available?

Thanks.

ラベル(2)
0 件の賞賛
返信
1 解決策
1,386件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Damon,

    1. non volatile storage

        Please go to page 636,  Program Flash IFR Map, there just has 64 program once field.

      If you want to use the unique serial number, the K50 has the Unique Identification Register, it contains the chip UID.

  2. FlexRAM

      You can find just MK50DX256CMC10 has the flexNVM and the FlexRAM, your chip is MK50DN512CMC10, it just has the Program flash.

  So, if the 64bits IFR is not enough, you may use the flash to store your configuration information.

Wish it helps you!


Have a great day,
Jingjing

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,386件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Damon,

    1. non volatile storage

        Please go to page 636,  Program Flash IFR Map, there just has 64 program once field.

      If you want to use the unique serial number, the K50 has the Unique Identification Register, it contains the chip UID.

  2. FlexRAM

      You can find just MK50DX256CMC10 has the flexNVM and the FlexRAM, your chip is MK50DN512CMC10, it just has the Program flash.

  So, if the 64bits IFR is not enough, you may use the flash to store your configuration information.

Wish it helps you!


Have a great day,
Jingjing

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信