MK20DX256VLH7 Programer/Debuger

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MK20DX256VLH7 Programer/Debuger

ソリューションへジャンプ
1,693件の閲覧回数
marhalloweenvt
Contributor I

Hello,

I am a newbeginer so this is maybe a dump question. My project uses MK20DX256VLH7 as a controller. I have search through google and found this ST-Link-V2 (http://sanphamdientugroup.tk/files/sanpham/49/1/jpg/mach-nap-cho-stm32-st-link-v2-mini.jpg ). Can i use this to program the mcu? If not which device i can use as a programer for this mcu?

Thanks for reading.

ラベル(1)
タグ(1)
1 解決策
1,534件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Minh Bui,

I'd highly recommend you to choose the following debugger.

2016-10-08_9-09-05.jpg


Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
1,535件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Minh Bui,

I'd highly recommend you to choose the following debugger.

2016-10-08_9-09-05.jpg


Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------