MCUXpresso Config Tools

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCUXpresso Config Tools

ソリューションへジャンプ
4,249件の閲覧回数
john71
Senior Contributor I

On the site in MCUXpresso Config Tools I choose New Configuration but I don't see in the list MK10FN1M0VLQ12. The chip is not supported in SDK?

0 件の賞賛
返信
1 解決策
3,964件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi

Yes, the K10_120MHz is the same platform product with K70_120MHz product.


Wish it helps.

Have a great day,
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
7 返答(返信)
3,964件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi

The KSDK software doesn't support MK10FN1M0VLQ12 product so far.  Sorry for that.

Customer could consider to use Processor Expert tool provided driver or related bare-metal project.


Wish it helps.

Have a great day,
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
3,964件の閲覧回数
john71
Senior Contributor I

Are the examples for K70 compatible to K10?

0 件の賞賛
返信
3,965件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi

Yes, the K10_120MHz is the same platform product with K70_120MHz product.


Wish it helps.

Have a great day,
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
3,964件の閲覧回数
john71
Senior Contributor I

I see. Thank you.

0 件の賞賛
返信
3,964件の閲覧回数
john71
Senior Contributor I

Well... I port the code from K70 project.

 

//#include "MK70F12.h" 

#include "MK10F12.h" 

#include "gpio.h"

void GPIO_Init(void)

{

//Enable Port clocks

SIM_SCGC5 |= ( SIM_SCGC5_PORTA_MASK | SIM_SCGC5_PORTB_MASK | SIM_SCGC5_PORTC_MASK | SIM_SCGC5_PORTD_MASK | SIM_SCGC5_PORTE_MASK | SIM_SCGC5_PORTF_MASK );

PORTB_PCR11 = PORT_PCR_MUX(1) | PORT_PCR_DSE_MASK;

GPIOB_PDDR |= 1<<11;

GPIOA_PDDR |= 1<<11;

GPIOA_PDDR |= 1<<12;

GPIOA_PDDR |= 1<<28;

GPIOA_PDDR |= 1<<29;

}

I get errors:


'GPIOA_PDDR' undeclared (first use in this function) 
'GPIOB_PDDR' undeclared (first use in this function) 
'PORTB_PCR11' undeclared (first use in this function) 
'SIM_SCGC5' undeclared (first use in this function) 

0 件の賞賛
返信
3,964件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi

You could use "make_new_project.exe" file to create new project based on [hello_world] demo.

I had tested to create a new project for K10 project with IAR IDE.

I need to modify the <common.h> file:

/*
 * Include the cpu specific header file
 */
#if (defined(CPU_MK70F120))
  #include "MK70F15.h"
#elif (defined(CPU_MK60F120))
  #include "MK70F15.h"
#elif (defined(CPU_MK10F120))
  #include "MK10F12.h"
#else
  #error "No valid CPU defined"
#endif

Then in <twr-k70f120m.h> file, change CPU type:

//#define CPU_MK70F120
#define CPU_MK10F120

Remove driver sdram folder with <sdram.c>&<sdram.h> files.

Then remove DDR initialization function call at <sysinit.c> file.

After that, I could pass compile of the project.


Wish it helps.

Have a great day,
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

3,964件の閲覧回数
john71
Senior Contributor I

Thank you.

0 件の賞賛
返信