LPTMR KL05

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPTMR KL05

3,118 Views
filipebranco
Contributor I

Hello,

I'm facing some problems using the KL05 FRDM board and i'm trying to toggle a pin using the LPTMR.
The LPTMR is clocked by the MCRIRCLK (32KHz) and i'm using a prescaler of 2 so the clock would be 16Khz. The result that i'm getting is 2msecs instead of 60uSecs.

Please find the code below:

#include "derivative.h" /* include peripheral declarations */

int main(void)

{

        SIM_SOPT1 |= (0<<18); //32K Oscillator clock

        SIM_SOPT1 |= (0<<19);

        SIM_SOPT1 = 0x00000000;

        SIM_SCGC5 |= (SIM_SCGC5_LPTMR_MASK | SIM_SCGC5_PORTB_MASK);// LPTMR gated PORTB

        PORTB_PCR8 |= 0x00000100;    // alternative pin mux selection //

        GPIOB_PDDR |= 0x00000100;    // pin direction //

        asm(" CPSIE i");

        NVIC_ICPR = 1 << (28);

        NVIC_ISER = 1 << (28);

       LPTMR0_CSR=0;

       LPTMR0_CSR |= 0x00000040; // HEX timer interrupt Enable

          /* Set the compare value to the number of ms to delay */

       LPTMR0_PSR = LPTMR_PSR_PCS(1)|LPTMR_PSR_PBYP_MASK;

       LPTMR0_CMR = 10; //Check what is the lowest we can get ?

          /* Start the timer */

       LPTMR0_CSR |= LPTMR_CSR_TEN_MASK;

}

void LPTimer_IRQHandler(void){

                  LPTMR0_CSR &= ~LPTMR_CSR_TEN_MASK;

                  LPTMR0_CSR |= LPTMR_CSR_TCF_MASK;

                  GPIOB_PTOR |= (1<<8);

                  LPTMR0_CSR |= LPTMR_CSR_TEN_MASK;

        }

If anyone knows why this is happening please let me know.


Many Thanks

Filipe Branco

Tags (3)
0 Kudos
Reply
4 Replies

2,775 Views
perlam_i_au
Senior Contributor I

I think you are setting by error the LPO 1kHz instead of the System oscillator, I suggest you to comment or delete the lines:

SIM_SOPT1 |= (0<<18); //32K Oscillator clock

SIM_SOPT1 |= (0<<19);

Here you are setting to use the LPO (OSC32KSEL= 11 = LPO 1kHz) this perfectly explain your 2msec period


Have a nice day :P,
Perla

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,775 Views
KL04_user
Contributor II

Hi,

isint he already clearing the settings set by

SIM_SOPT1 |= (0<<18);   

SIM_SOPT1 |= (0<<19);

by the third line

SIM_SOPT1 = 0x00000000; and selecting System oscillator (OSC32KCLK)??

Also, these lines

SIM_SOPT1 |= (0<<18);   

SIM_SOPT1 |= (0<<19);

have no effect as 0 is being shifted so many times!!!

Am also struck with a similar problem. Any suggestions would be helpful..

Thanks in advance

0 Kudos
Reply

2,775 Views
mjbcswitzerland
Specialist V

Hi

SIM_SOPT1 is relevant for the RTC and not the LPTMR.

The LPTMR clock source is defined in LPTMR0_PSR.

If using the external oscillator as clock input, the external oscillator input connection must also be enabled in OSC0_CR (irrespective of whether the oscillator is running or not).

Therefore:

        OSC0_CR |= (OSC_CR_ERCLKEN | OSC_CR_EREFSTEN);           // enable the external reference clock and keep it enabled in stop mode
       

LPTMR0_PSR = (LPTMR_PSR_PCS_OSC0ERCLK | LPTMR_PSR_PBYP);

This will clock the LPTRM from the oscillator input.

Regards

Mark

0 Kudos
Reply

2,775 Views
KL04_user
Contributor II

Thanks Mark.. That explains a lot.

0 Kudos
Reply