Errata for mask 1N96F clarification (I2C repeated start)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Errata for mask 1N96F clarification (I2C repeated start)

跳至解决方案
2,060 次查看
jrychter
Contributor V

Errata document for mask 1N96F states:

e6070: I2C: Repeat start cannot be generated if the I2Cx_F[MULT] field is set to a non- zero value

The following workaround is proposed:

2) Temporarily set I2Cx_F [MULT] to zero immediately before setting the Repeat START bit in the I2C C1 register (I2Cx_C1[RSTA]=1) and restore the I2Cx_F [MULT] field to the original value after the repeated start has occurred

What does "after the repeated start has occurred" mean? Does this mean I can restore I2Cx_F[MULT] field immediately after I write 1 to RSTA?

In other words, is the following code OK?

          f_register = I2C_F_REG(i2c_base_ptr);

          I2C_F_REG(i2c_base_ptr) = (f_register & 0x3f);

          I2C_C1_REG(i2c_base_ptr) |= I2C_C1_RSTA_MASK;

          I2C_F_REG(i2c_base_ptr) = f_register;



标签 (1)
0 项奖励
回复
1 解答
1,732 次查看
perlam_i_au
Senior Contributor I

Yes, it seems your code is correct.

在原帖中查看解决方案

0 项奖励
回复
4 回复数
1,732 次查看
perlam_i_au
Senior Contributor I

Hello Jan:

Well the repeat start is used for redirect your messages as master to a different slave without releasing the bus, then this means that you can use the lines you described to set desired value for MULT once you have generated the Repeated Start.

Please check on 38.4.1.5 Repeated START signal and Figure 38-38. I2C bus transmission signals on the reference manual KL25P80M48SF0RM which I used as example.


Have a nice day,
Perla Moncada

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,732 次查看
jrychter
Contributor V

To clarify: I wasn't sure if the RSTA bit controlled the output latch directly, e.g. if writing to it caused the restart to be generated immediately, or after a write to the data register, just before a new address byte is transmitted.

From your answer, I understand that writing to RSTA immediately generates a restart condition, so my code is OK. Please correct me if this is not the case. Thanks!

0 项奖励
回复
1,733 次查看
perlam_i_au
Senior Contributor I

Yes, it seems your code is correct.

0 项奖励
回复
1,732 次查看
jrychter
Contributor V

Thank you, appreciate the help!

0 项奖励
回复