LLWU Pin Configuration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LLWU Pin Configuration

ソリューションへジャンプ
3,901件の閲覧回数
ttocsmi
Contributor I

I do not plan on using wake-up functionality in my application.  Are there any special considerations I should be aware of if I would like to use (for example) the PTE1/LLWU_P0 pin for general purpose IO?  Is this even possible?

Thank you.

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
2,499件の閲覧回数
apanecatl
Senior Contributor II

As long as the PTE1 is not configured as a wakeup source by enabling the corresponding bit in LLWU Pin Enable 1 Register (LLWU_PE1_WUPE0), you can use it as a GPIO.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,500件の閲覧回数
apanecatl
Senior Contributor II

As long as the PTE1 is not configured as a wakeup source by enabling the corresponding bit in LLWU Pin Enable 1 Register (LLWU_PE1_WUPE0), you can use it as a GPIO.

0 件の賞賛
返信
2,499件の閲覧回数
jvasil
Contributor III

Actually, I believe you can use the GPIO functionality and the LLWU functionality at the same time.

0 件の賞賛
返信
2,499件の閲覧回数
apanecatl
Senior Contributor II

Actually you are correct, both functions can be used at the same time. my bad...

0 件の賞賛
返信