LLWU Pin Configuration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LLWU Pin Configuration

Jump to solution
3,949 Views
ttocsmi
Contributor I

I do not plan on using wake-up functionality in my application.  Are there any special considerations I should be aware of if I would like to use (for example) the PTE1/LLWU_P0 pin for general purpose IO?  Is this even possible?

Thank you.

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
2,547 Views
apanecatl
Senior Contributor II

As long as the PTE1 is not configured as a wakeup source by enabling the corresponding bit in LLWU Pin Enable 1 Register (LLWU_PE1_WUPE0), you can use it as a GPIO.

View solution in original post

0 Kudos
Reply
3 Replies
2,547 Views
apanecatl
Senior Contributor II

As long as the PTE1 is not configured as a wakeup source by enabling the corresponding bit in LLWU Pin Enable 1 Register (LLWU_PE1_WUPE0), you can use it as a GPIO.

0 Kudos
Reply
2,547 Views
jvasil
Contributor III

Actually, I believe you can use the GPIO functionality and the LLWU functionality at the same time.

0 Kudos
Reply
2,547 Views
apanecatl
Senior Contributor II

Actually you are correct, both functions can be used at the same time. my bad...

0 Kudos
Reply