LLWU Pin Configuration

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LLWU Pin Configuration

跳至解决方案
3,790 次查看
ttocsmi
Contributor I

I do not plan on using wake-up functionality in my application.  Are there any special considerations I should be aware of if I would like to use (for example) the PTE1/LLWU_P0 pin for general purpose IO?  Is this even possible?

Thank you.

标签 (1)
标记 (2)
0 项奖励
回复
1 解答
2,388 次查看
apanecatl
Senior Contributor II

As long as the PTE1 is not configured as a wakeup source by enabling the corresponding bit in LLWU Pin Enable 1 Register (LLWU_PE1_WUPE0), you can use it as a GPIO.

在原帖中查看解决方案

0 项奖励
回复
3 回复数
2,389 次查看
apanecatl
Senior Contributor II

As long as the PTE1 is not configured as a wakeup source by enabling the corresponding bit in LLWU Pin Enable 1 Register (LLWU_PE1_WUPE0), you can use it as a GPIO.

0 项奖励
回复
2,388 次查看
jvasil
Contributor III

Actually, I believe you can use the GPIO functionality and the LLWU functionality at the same time.

0 项奖励
回复
2,388 次查看
apanecatl
Senior Contributor II

Actually you are correct, both functions can be used at the same time. my bad...

0 项奖励
回复