KinetisL Sample Code running on Codewarrior

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

KinetisL Sample Code running on Codewarrior

跳至解决方案
1,761 次查看
mithunp_s
Contributor III

Hi ,

I've extracted sample codes from KL25_SC.exe, I'm refering to LQRUG_uart_ex1 example.

When I try to Import this project code warrior is giving error saying "No Projects are found to Import", next when I manually open this folder (Kinetis L Sample Code\kl25_sc\klxx-sc-baremetal\src\projects) there are only two files available LQRG_uart_ex1.c & isr.h.

Please help how to make this example work on code warrior, If I have to add any other dependencies how to add, please brief me on this.

I can also see all these example projects provided in the barematel folder give the same problem,

Regards

Mithun

0 项奖励
回复
1 解答
1,530 次查看
apanecatl
Senior Contributor II

The problem there is the projects you can't open are only available for IAR and KEIL, we have plans to migrate many of them to CodeWarrior but we haven't defined a specific date to do so.

Sorry about this.

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,531 次查看
apanecatl
Senior Contributor II

The problem there is the projects you can't open are only available for IAR and KEIL, we have plans to migrate many of them to CodeWarrior but we haven't defined a specific date to do so.

Sorry about this.

0 项奖励
回复