KinetisL Sample Code running on Codewarrior

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KinetisL Sample Code running on Codewarrior

Jump to solution
1,906 Views
mithunp_s
Contributor III

Hi ,

I've extracted sample codes from KL25_SC.exe, I'm refering to LQRUG_uart_ex1 example.

When I try to Import this project code warrior is giving error saying "No Projects are found to Import", next when I manually open this folder (Kinetis L Sample Code\kl25_sc\klxx-sc-baremetal\src\projects) there are only two files available LQRG_uart_ex1.c & isr.h.

Please help how to make this example work on code warrior, If I have to add any other dependencies how to add, please brief me on this.

I can also see all these example projects provided in the barematel folder give the same problem,

Regards

Mithun

0 Kudos
Reply
1 Solution
1,675 Views
apanecatl
Senior Contributor II

The problem there is the projects you can't open are only available for IAR and KEIL, we have plans to migrate many of them to CodeWarrior but we haven't defined a specific date to do so.

Sorry about this.

View solution in original post

0 Kudos
Reply
1 Reply
1,675 Views
apanecatl
Senior Contributor II

The problem there is the projects you can't open are only available for IAR and KEIL, we have plans to migrate many of them to CodeWarrior but we haven't defined a specific date to do so.

Sorry about this.

0 Kudos
Reply