KinetisL Sample Code running on Codewarrior

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KinetisL Sample Code running on Codewarrior

ソリューションへジャンプ
1,907件の閲覧回数
mithunp_s
Contributor III

Hi ,

I've extracted sample codes from KL25_SC.exe, I'm refering to LQRUG_uart_ex1 example.

When I try to Import this project code warrior is giving error saying "No Projects are found to Import", next when I manually open this folder (Kinetis L Sample Code\kl25_sc\klxx-sc-baremetal\src\projects) there are only two files available LQRG_uart_ex1.c & isr.h.

Please help how to make this example work on code warrior, If I have to add any other dependencies how to add, please brief me on this.

I can also see all these example projects provided in the barematel folder give the same problem,

Regards

Mithun

ラベル(2)
0 件の賞賛
返信
1 解決策
1,676件の閲覧回数
apanecatl
Senior Contributor II

The problem there is the projects you can't open are only available for IAR and KEIL, we have plans to migrate many of them to CodeWarrior but we haven't defined a specific date to do so.

Sorry about this.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,676件の閲覧回数
apanecatl
Senior Contributor II

The problem there is the projects you can't open are only available for IAR and KEIL, we have plans to migrate many of them to CodeWarrior but we haven't defined a specific date to do so.

Sorry about this.

0 件の賞賛
返信