Kinetis K70 Pin-pin compatible ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Kinetis K70 Pin-pin compatible ?

Jump to solution
2,090 Views
joelesco
Contributor III

Hi !

I would like to know if all the K70 family is pin-pin compatible ? Because I found some information conflicting ! In the K70 product brief they write " The K70 is available with 512 KB or 1 MB of flash memory in 196- and 256-pin MAPBGA packages." but when i check on K70_120: Kinetis K70 Graphic LCD 120/150 MHz MCUs  all the familly has 256 pin count.

Thanks !!!!!!!!!!!!!

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
1,925 Views
soledad
NXP Employee
NXP Employee

Hi,

The 196MAPBGA package was removed from all Kinetis products family in 5-Mar,2012.

Regards,

Sol

View solution in original post

0 Kudos
Reply
3 Replies
1,925 Views
joelesco
Contributor III

thank you soledad! So all the K70 familly is pin pin compatible? I mean if i want to change the µC with an other with more capacity its possible ?

thanks a lot !

0 Kudos
Reply
1,925 Views
soledad
NXP Employee
NXP Employee

Yes, all the K70 family is pin-pin compatible.

Regards :smileywink:

Sol

0 Kudos
Reply
1,926 Views
soledad
NXP Employee
NXP Employee

Hi,

The 196MAPBGA package was removed from all Kinetis products family in 5-Mar,2012.

Regards,

Sol

0 Kudos
Reply