Kinetis K24 Clock

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,866件の閲覧回数
smathad
Contributor II

Hello all,

I am working on the NXP K24 clock. I see that there are multiple clocks available to choose from. While the reference manual does give some description about the clocks, it is very generic.

I did not find a document explaining me the exact use of each of these clocks. 

Can somebody explain to me the use case of each of these clocks? I have listen them below. 

  1. MCGIRCLK
  2. MCGFFCLK
  3. Core/System Clocks
  4. Bus clock
  5. FlexBus clock
  6. Flash Clock
  7. MCGPLLCLK/MCGFLLCLK
  8. OSCERCLK
  9. ERCLK32K
  10. LPO
  11. RTC_CLKOUT

Thanks 

Sachin

ラベル(1)
0 件の賞賛
返信
1 解決策
3,799件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Sachin Mathad ,

   Thanks for your interest in the NXP kinetis product, I would like to provide service for you.

   About the use case of each clock, in fact, you can refer to the MK24 reference manual , Chapter 5 Clock Distribution.

   5.4 Clock definitions, this chapter told you each clock usage.

   Table 5-2. Module clocks, told you each module clock situation.

   Please read the MK24 reference manual clock distribution chapter at first.

https://www.nxp.com/webapp/Download?colCode=K24P144M120SF5RM 

If you still have questions about it, please kindly let me know.

Have a great day,
Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

   

   

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
3,800件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Sachin Mathad ,

   Thanks for your interest in the NXP kinetis product, I would like to provide service for you.

   About the use case of each clock, in fact, you can refer to the MK24 reference manual , Chapter 5 Clock Distribution.

   5.4 Clock definitions, this chapter told you each clock usage.

   Table 5-2. Module clocks, told you each module clock situation.

   Please read the MK24 reference manual clock distribution chapter at first.

https://www.nxp.com/webapp/Download?colCode=K24P144M120SF5RM 

If you still have questions about it, please kindly let me know.

Have a great day,
Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

   

   

0 件の賞賛
返信
3,799件の閲覧回数
smathad
Contributor II

Hi Kerry, 

Thank you for your response. 

I did find that table helpful. 

Can you please let me know the difference between bus interface clock, internal clock and I/o interface clock in that table? 

 table 5-2.PNG

Regards,

Sachin 

0 件の賞賛
返信
3,799件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Sachin Mathad,

  You are welcome!

   Bus interface clock, you can consider the related module register control clock.

   Internal clocks, you can consider it as the module clock, now take LPTMR as an example

pastedImage_1.png

pastedImage_3.png

You can find the LPTMR internal clocks is the module clock.

 I/o interface clock is the clock which is input or output to the related IO pins.

Wish it helps you!

If you still have questions about it, please kindly let me know.

Have a great day,
Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信