Kinetis K22 TWR-K22F120M + TWR-SER2 USB High-Speed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Kinetis K22 TWR-K22F120M + TWR-SER2 USB High-Speed

Jump to solution
1,930 Views
nbgatgi
Contributor IV

Does the enhanced serial tower board (TWR-SER2) make high-speed (HS) USB possible with the Kinetis K22 tower board (TWR-K22F120M)?

Labels (2)
0 Kudos
Reply
1 Solution
1,801 Views
mjbcswitzerland
Specialist V

Nick

The K22 has full speed OTG and not HS USB so it can't be used with the HS tranceiver on the SER2 board.

You will need a K26 for HS USB.

Regards

Mark

View solution in original post

1 Reply
1,802 Views
mjbcswitzerland
Specialist V

Nick

The K22 has full speed OTG and not HS USB so it can't be used with the HS tranceiver on the SER2 board.

You will need a K26 for HS USB.

Regards

Mark