Kinetis K sector erase endurance

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Kinetis K sector erase endurance

1,516件の閲覧回数
dkh
NXP Employee
NXP Employee

Hello Support,

If I am writing and erasing 1 or 2 sectors of program flash heavily will it impact the endurance or reliability of the the other sectors or blocks of flash ?

I want to write small blocks of data to a sector appending them until it is full then erase the sector hoping to maximize

the endurance.

Will this method improve the endurance assuming that the erase sector function is what impacts the endurance ?

Regards,

0 件の賞賛
返信
1 返信

1,339件の閲覧回数
dkh
NXP Employee
NXP Employee

Other parts of the flash should not be impacted. The endurance is for each flash page, so you can wear level by moving data to a new page when your current page is suspected to be close to the end of its life.

You can append but make sure you aren’t overprogramming (programming a flash word that is not in an erased state) attempt to avoid erase cycles as that will cause a different set of issues.

MH

0 件の賞賛
返信