Kinetis K sector erase endurance

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Kinetis K sector erase endurance

1,514 Views
dkh
NXP Employee
NXP Employee

Hello Support,

If I am writing and erasing 1 or 2 sectors of program flash heavily will it impact the endurance or reliability of the the other sectors or blocks of flash ?

I want to write small blocks of data to a sector appending them until it is full then erase the sector hoping to maximize

the endurance.

Will this method improve the endurance assuming that the erase sector function is what impacts the endurance ?

Regards,

0 Kudos
Reply
1 Reply

1,337 Views
dkh
NXP Employee
NXP Employee

Other parts of the flash should not be impacted. The endurance is for each flash page, so you can wear level by moving data to a new page when your current page is suspected to be close to the end of its life.

You can append but make sure you aren’t overprogramming (programming a flash word that is not in an erased state) attempt to avoid erase cycles as that will cause a different set of issues.

MH

0 Kudos
Reply