Kinetis Bootloader that supports the K70 device

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Kinetis Bootloader that supports the K70 device

1,140件の閲覧回数
ECE
Contributor I

I see from the NXP web site that the Kinetis Bootloader v2 does not support the K70 device.  Is there work being done on the porting of this application to the K70?  If so, is there a date that I can expect this to be available and/or is a pre-release available?

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,001件の閲覧回数
mjbcswitzerland
Specialist V

Hi Bill

You can get KBOOT compatible UART/USB code for the K70 at http://www.utasker.com/kinetis/TWR-K70F120M.html

This allows you to build with IAR, Keil, KDS, CW, Crossworks, Green Hills etc. and optionally mix KBOOT mode with USB-MSD, Memory stick, Ethernet, SD-card etc. according to http://www.utasker.com/docs/uTasker/uTaskerSerialLoader.PDF

Regards

Mark

0 件の賞賛
返信