Kinetis Bootloader that supports the K70 device

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Kinetis Bootloader that supports the K70 device

830 Views
ECE
Contributor I

I see from the NXP web site that the Kinetis Bootloader v2 does not support the K70 device.  Is there work being done on the porting of this application to the K70?  If so, is there a date that I can expect this to be available and/or is a pre-release available?

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

691 Views
mjbcswitzerland
Specialist V

Hi Bill

You can get KBOOT compatible UART/USB code for the K70 at http://www.utasker.com/kinetis/TWR-K70F120M.html

This allows you to build with IAR, Keil, KDS, CW, Crossworks, Green Hills etc. and optionally mix KBOOT mode with USB-MSD, Memory stick, Ethernet, SD-card etc. according to http://www.utasker.com/docs/uTasker/uTaskerSerialLoader.PDF

Regards

Mark

0 Kudos
Reply