Kinetis Bootloader that supports the K70 device

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Kinetis Bootloader that supports the K70 device

1,163 次查看
ECE
Contributor I

I see from the NXP web site that the Kinetis Bootloader v2 does not support the K70 device.  Is there work being done on the porting of this application to the K70?  If so, is there a date that I can expect this to be available and/or is a pre-release available?

标签 (1)
标记 (1)
0 项奖励
回复
1 回复

1,024 次查看
mjbcswitzerland
Specialist V

Hi Bill

You can get KBOOT compatible UART/USB code for the K70 at http://www.utasker.com/kinetis/TWR-K70F120M.html

This allows you to build with IAR, Keil, KDS, CW, Crossworks, Green Hills etc. and optionally mix KBOOT mode with USB-MSD, Memory stick, Ethernet, SD-card etc. according to http://www.utasker.com/docs/uTasker/uTaskerSerialLoader.PDF

Regards

Mark

0 项奖励
回复