KV58, SPI Master

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KV58, SPI Master

1,075件の閲覧回数
a8Chcx
Contributor V

Hi,

I am using SPI sample code "dspi_polling_b2b_transfer_master.c" for KV58.

I am using SPI0, PCS0 and PCS1 to control my SPI slave devices. I can't get the right value from slave device.

But, I control SPI0 and SPI1 by using GPIO, it works fine.

I checked that PCS0 and PCS1 are going to LOW/HIGH in both cases.

Can anyone tell me where I need to adjust to make it work in both cases?

Thanks,

Christie

ラベル(1)
0 件の賞賛
返信
0 返答(返信)