KV5 MCGPLLCLK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KV5 MCGPLLCLK

2,743件の閲覧回数
ohiogt
Contributor III

The datasheet for the MKV5X has the following values in Table 17 for the PLL:

Reference Frequency Range: 8 to 16 MHz

Ipll @ 176 MHz: 2.8 mA (Note says fpll_ref = 8 MHz, VDIV = 22, 8 * 22 = 176 MHz)

Ipll @ 360 MHz: 4.7 mA (Note says fpll_ref = 8 MHz, VDIV = 45, 8 * 45 = 360 MHz)

This seems to indicate that the feedback for the PLL comes directly from the VCO output.

However, this contradicts Figure 32-1 in the reference manual.  This figure shows the feedback being derived from the fixed divide-by-2 MCGPLLCLK output.  I confirmed using the FlexBus clock output pin and the PIT that the PLL N-divider appears to actually be connected to MCGPLLCLK2X.  Can you please confirm if the following markup is correct? 

9-18-2017 5-10-17 PM.jpg

ラベル(1)
タグ(3)
0 件の賞賛
返信
3 返答(返信)

2,519件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Shawn,

If above figure is correct, the VCO output frqeuency(MCGPLLCLK2X) is 8MHz*VDIV*2, MCGPLLCLK is 8MHz*VDIV.

I will test it tomorrow, can you post the PLL setting code here?

BR

Xiangjun Rong

0 件の賞賛
返信

2,519件の閲覧回数
ohiogt
Contributor III

Xiangjun,

Yes, I believe that's correct.  In my application I have a 10 MHz PLL reference frequency and would like MCGPLLCLK/MCGOUTCLK to operate at 160 MHz.  In the original Figure 32-1, it led me to believe VDIV should be set to 16.  I actually have to set it to 32, meaning the VDIV input must actually be connected directly to the VCO output (MCGPLLCLK2X).  Code is below:

// -----------------------------------------------------------------

//

// Name: InitOSC

//

// Description:

//

// Enables the external reference and sets clock dividers

// to initial low speed values for boot.

//

// Input parameters:

// None.

//

// Returned value:

// None.

//

// Algorithm:

// 1) Set low speed system clock dividers:

// Core clock: 1

// Bus clock: 6

// FlexBus clock: 6

// Flash clock: 6

// 2) Enable external oscillator

// 3) Set oscillator divider to 1 (40 MHz / 1 = 40 MHz) for

// the OSCERCLK output.

//

// Special Notes:

// None.

//

// -----------------------------------------------------------------

void initOSC(void)

{

uint32_t tmp32 = 0x00000000;

tmp32 = SIM->CLKDIV1;

tmp32 &= ~(SIM_CLKDIV1_OUTDIV1_MASK | SIM_CLKDIV1_OUTDIV2_MASK |

SIM_CLKDIV1_OUTDIV3_MASK | SIM_CLKDIV1_OUTDIV4_MASK);

tmp32 |= (SIM_CLKDIV1_OUTDIV1(0x01) | SIM_CLKDIV1_OUTDIV2(0x05) |

SIM_CLKDIV1_OUTDIV3(0x05) | SIM_CLKDIV1_OUTDIV4(0x05));

SIM->CLKDIV1 = tmp32;

OSC0->CR &= ~(OSC_CR_EREFSTEN_MASK | OSC_CR_SC2P_MASK | OSC_CR_SC4P_MASK |

OSC_CR_SC8P_MASK | OSC_CR_SC16P_MASK);

OSC0->CR |= OSC_CR_ERCLKEN_MASK;

OSC0->DIV &= ~(OSC_DIV_ERPS_MASK);

OSC0->DIV |= OSC_DIV_ERPS(0x0);

}

// -----------------------------------------------------------------

//

// Name: InitMCG

//

// Description:

//

// Initializes the clock generator module for high speed PLL operation

// based on the external reference.

//

// Input parameters:

// None.

//

// Returned value:

// None.

//

// Algorithm:

// 1) Zero out trim.

// 2) Set DCO for low speed range and 0 trim.

// 3) Select OSCCLK0 for MCG FLL external reference (Default C7 setting on KV5).

// 4) Disable loss of lock monitors.

// 5) Set the MCG range for very high frequency oscillator.

// 6) Set FLL clock source to external reference with divider of 1280. This

// results in 40 MHz / 1280 = 31.250 kHz for the FLL. This

// clock is based on OSCCLK.

// 7) Set MCGOUTCLK source to external reference.

// 8) Wait for status to indicate external reference for FLL.

// 9) Wait for status to indicate external reference for MCGOUTCLK.

// 10) Enable PLL and set reference divider to 4, so 40 MHz / 4 = 10 MHz.

// 11) Enable PLL as MCGOUTCLK. Set feedback divider to 32, so (32 * 10 MHz) / 2 = 160 MHz.

// 12) Wait for status to indicate PLL selected.

// 13) Wait for status to indicate PLL locked.

// 14) Select PLL output for MCGOUTCLK.

// 15) Wait for status to indicate PLL is active clock.

//

// Special Notes:

// None.

//

// -----------------------------------------------------------------

void initMCG(void)

{

MCG->C3 = 0x00;

MCG->C4 = 0x00;

MCG->C8 &= ~(MCG_C8_LOLRE_MASK);

MCG->C2 = MCG_C2_RANGE(2U);

MCG->C1 = (MCG_C1_CLKS(2U) | MCG_C1_FRDIV(6U));

while ((MCG->S & MCG_S_IREFST_MASK) != 0x00)

{

}

while ((MCG->S & MCG_S_CLKST_MASK) != 0x08)

{

}

MCG->C5 = (MCG_C5_PLLCLKEN0_MASK | MCG_C5_PRDIV0(3U));

MCG->C6 = (MCG_C6_PLLS_MASK | MCG_C6_VDIV0(16U));

while ((MCG->S & MCG_S_PLLST_MASK) != 0x20)

{

}

while ((MCG->S & MCG_S_LOCK0_MASK) != 0x40)

{

}

MCG->C1 &= ~(MCG_C1_CLKS_MASK);

while ((MCG->S & MCG_S_CLKST_MASK) != 0x0C)

{

}

}

void initRUN(void)

{

uint32_t tmp32 = 0x00000000;

SMC->PMPROT &= ~(SMC_PMPROT_AHSRUN_MASK | SMC_PMPROT_AVLP_MASK | SMC_PMPROT_AVLLS_MASK);

SMC->PMCTRL &= ~(SMC_PMCTRL_RUNM_MASK);

while ((SMC->PMSTAT & SMC_PMSTAT_PMSTAT_MASK) != 0x01)

{

}

tmp32 = SIM->CLKDIV1;

tmp32 &= ~(SIM_CLKDIV1_OUTDIV1_MASK | SIM_CLKDIV1_OUTDIV2_MASK |

SIM_CLKDIV1_OUTDIV3_MASK | SIM_CLKDIV1_OUTDIV4_MASK);

tmp32 |= (SIM_CLKDIV1_OUTDIV1(0x00) | SIM_CLKDIV1_OUTDIV2(0x01) |

SIM_CLKDIV1_OUTDIV3(0x07) | SIM_CLKDIV1_OUTDIV4(0x07));

SIM->CLKDIV1 = tmp32;

}

0 件の賞賛
返信

2,519件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Shawn,

Okay, i see, the /2 divider is not in the feedback loop as the figure.

BR

Xiangjun Rong

0 件の賞賛
返信