KM35 external voltage reference

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

KM35 external voltage reference

跳至解决方案
3,310 次查看
NArn
Contributor II

Hello,

What is the maximum voltage of an external voltage reference for MKM35Z512VLQ7? I am considering using a REF7012, which is 1.25 V +- 0.025%, 2ppm/C.

Best regards

Niclas

0 项奖励
回复
1 解答
3,257 次查看
NArn
Contributor II

So, no reason to spend any more time in this forum? If the NXP staff can only provide information that I should manage to find myself in the published material, what is the point?

在原帖中查看解决方案

0 项奖励
回复
4 回复数
3,268 次查看
NArn
Contributor II

Please let me repeat my question: What is the maximum voltage of an external voltage reference for MKM35Z512VLQ7?

0 项奖励
回复
3,261 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi @NArn ,

No such data. I think it should be 1.2V.

 

Regards,

Jing

0 项奖励
回复
3,258 次查看
NArn
Contributor II

So, no reason to spend any more time in this forum? If the NXP staff can only provide information that I should manage to find myself in the published material, what is the point?

0 项奖励
回复
3,289 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi @NArn ,

As the NOTE of Figure 34-1 in RM says, you can use externally supplied VREF. But there is no data shows what if external VREF is 1.25V, not 1.2V. In fact, most of people use internal VREF. It is good enough.

 

Regards,

Jing

0 项奖励
回复