KM35 external voltage reference

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KM35 external voltage reference

ソリューションへジャンプ
3,524件の閲覧回数
NArn
Contributor II

Hello,

What is the maximum voltage of an external voltage reference for MKM35Z512VLQ7? I am considering using a REF7012, which is 1.25 V +- 0.025%, 2ppm/C.

Best regards

Niclas

0 件の賞賛
返信
1 解決策
3,471件の閲覧回数
NArn
Contributor II

So, no reason to spend any more time in this forum? If the NXP staff can only provide information that I should manage to find myself in the published material, what is the point?

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
3,482件の閲覧回数
NArn
Contributor II

Please let me repeat my question: What is the maximum voltage of an external voltage reference for MKM35Z512VLQ7?

0 件の賞賛
返信
3,475件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi @NArn ,

No such data. I think it should be 1.2V.

 

Regards,

Jing

0 件の賞賛
返信
3,472件の閲覧回数
NArn
Contributor II

So, no reason to spend any more time in this forum? If the NXP staff can only provide information that I should manage to find myself in the published material, what is the point?

0 件の賞賛
返信
3,503件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi @NArn ,

As the NOTE of Figure 34-1 in RM says, you can use externally supplied VREF. But there is no data shows what if external VREF is 1.25V, not 1.2V. In fact, most of people use internal VREF. It is good enough.

 

Regards,

Jing

0 件の賞賛
返信