KL36: VDD vs Frequency

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KL36: VDD vs Frequency

Jump to solution
1,846 Views
BasePointer
Contributor II

Is there any limitation for CPU frequency executing code from flash vs VDD?

For example: Is maximum speed possible at 1.7V?

10x.

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,718 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Mehmet Fide,

No, there is no limitation for CPU freq across the VDD range, but only the power mode has the limitation on clock freq, please kindly refer to the following for details.

1.png


Have a great day,
B.R
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,719 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Mehmet Fide,

No, there is no limitation for CPU freq across the VDD range, but only the power mode has the limitation on clock freq, please kindly refer to the following for details.

1.png


Have a great day,
B.R
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply