KL36: VDD vs Frequency

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KL36: VDD vs Frequency

ソリューションへジャンプ
1,912件の閲覧回数
BasePointer
Contributor II

Is there any limitation for CPU frequency executing code from flash vs VDD?

For example: Is maximum speed possible at 1.7V?

10x.

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,784件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Mehmet Fide,

No, there is no limitation for CPU freq across the VDD range, but only the power mode has the limitation on clock freq, please kindly refer to the following for details.

1.png


Have a great day,
B.R
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,785件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Mehmet Fide,

No, there is no limitation for CPU freq across the VDD range, but only the power mode has the limitation on clock freq, please kindly refer to the following for details.

1.png


Have a great day,
B.R
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信