KL26z256 core and peripheral header file download for use in eclipse

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KL26z256 core and peripheral header file download for use in eclipse

Jump to solution
1,491 Views
nurichard
Contributor III

Hello,

Can anyone point me to where I can download the KL26z256 ARM core and peripheral header files so that I can incorporate them into an eclipse project.

Thank you,

Richard

Labels (1)
1 Solution
1,248 Views
al_muir
NXP Employee
NXP Employee

The KL26 demo code is now actually available and can be downloaded at:

http://cache.freescale.com/files/32bit/software/FRDM-KL26Z_SC.exe

The header file is actually slightly different from the KL25 to take account of the added features of the KL26 device family.

View solution in original post

2 Replies
1,248 Views
nurichard
Contributor III

For anyone else interested; Freescale support responded with:

the core and peripheral C header files of KL26Z256VMC4 is the same as KL25, so you can use the files in the KL25 demo code.

The demo code download link is :

http://cache.freescale.com/files/32bit/software/KL25_SC.exe?fpsp=1&WT_TYPE=Lab and Test Software&WT_VENDOR=FREESCALE&WT_FILE_FORMAT=exe&WT_ASSET=Downloads&sr=44

0 Kudos
Reply
1,249 Views
al_muir
NXP Employee
NXP Employee

The KL26 demo code is now actually available and can be downloaded at:

http://cache.freescale.com/files/32bit/software/FRDM-KL26Z_SC.exe

The header file is actually slightly different from the KL25 to take account of the added features of the KL26 device family.