Hello,
Can anyone point me to where I can download the KL26z256 ARM core and peripheral header files so that I can incorporate them into an eclipse project.
Thank you,
Richard
解決済! 解決策の投稿を見る。
The KL26 demo code is now actually available and can be downloaded at:
http://cache.freescale.com/files/32bit/software/FRDM-KL26Z_SC.exe
The header file is actually slightly different from the KL25 to take account of the added features of the KL26 device family.
For anyone else interested; Freescale support responded with:
the core and peripheral C header files of KL26Z256VMC4 is the same as KL25, so you can use the files in the KL25 demo code.
The demo code download link is :
http://cache.freescale.com/files/32bit/software/KL25_SC.exe?fpsp=1&WT_TYPE=Lab and Test Software&WT_VENDOR=FREESCALE&WT_FILE_FORMAT=exe&WT_ASSET=Downloads&sr=44
The KL26 demo code is now actually available and can be downloaded at:
http://cache.freescale.com/files/32bit/software/FRDM-KL26Z_SC.exe
The header file is actually slightly different from the KL25 to take account of the added features of the KL26 device family.